Smart Power Switches Forum Discussions
text.format{('custom.tabs.no.results')}
英飞凌工程师你好:
请问有没有16管脚的与BTS7040功能相近、规格相近的产品呢,想用来与我们现阶段使用的别家公司16管脚的同类产品进行替代可行性评估。
The BTH50030 is ideal for a project I'm involved with. Could one of the Infineon team members please give an approximate ETA date for these to be available through Digikey, Element14 etc? Thanks
Show LessHey,
I have to use BTS70012-1ESP in the replacement of BTS70020-EPP.
I have some doubt regarding calibration factor and derating curve table.
We are using Pic16u33 mcu which does not support floating point unit.
so our all the calculation is in Integer format.
how can I calibrate the 10 bit ADC sample which is coming from BTS70012 Is pin.
how to convert it into the voltage form because , I need to read the current.
Derating curve table i need to create but, I don't know how to calculate.
Derating curve table will be in term of I vs Time.
for 5 amp, 10 amp, 15 amp, 20 amp current what will be the floating numbers.
for reference in term of BTS70020 it is ....
Please response,
I will be always thankful of yours.
Hello, if the BTS724G channels are used independently and 4 channels are opened at the same time, can each channel reach 3.3A with load? Are there any other restrictions?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E6%99%BA%E8%83%BD%E7%94%B5%E6%BA%90%E5%BC%80%E5%85%B3/BTS724G%E5%B8%A6%E8%B4%9F%E8%BD%BD%E8%83%BD%E5%8A%9B/td-p/669756
Show Less英飞凌工程师你好:
在选用highside switch时,英飞凌具有各种系列的产品,在各系列的应用框图中,GND管脚的外围网络连接会有不同,能简单介绍一下其中原因吗
1. Can BTS7010-2EPA use PWM signals to drive 2. The load is an inductive load.
3. For the 2-channel chip you currently want to use, whether the chip load current is the sum of the current of the two channels.
Looking forward to clarifying, thank you
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E6%99%BA%E8%83%BD%E7%94%B5%E6%BA%90%E5%BC%80%E5%85%B3/BTS7010-2EPA%E9%A9%B1%E5%8A%A8%E9%97%AE%E9%A2%98/td-p/668095
Show LessWhat is the ON control delay time of the internal MOSFET when IN is set to High?
I checked the specifications for Switch-ON Delay (tON(DELAY)) and Switch-ON Time (tON) on the data sheet. I think that this parameter varies depending on the load. On the other hand, my understanding is that the delay in the IPD's internal circuit does not vary depending on the load conditions.
We have received inquiries from end customers regarding the time it takes for IPD to turn ON after setting IN to High.
I understand that Switch-ON Delay and Switch-ON Time vary depending on the load conditions, so the answer is that it depends on the load conditions. On the other hand, I think that IPD internal delay does not vary depending on load conditions, so I would like to separate the factors that cause variation and those that do not, and explain both to them.
Thanks,
Tetsuo
Show LessDear colleagues,
Please advice a replacement for IPS1041RPbF / AUIPS1041R.
With the following requirements:
1. TO252-3
2. Overcurrent shutdown (but not overcurrent limit) 3A...4A
3. Max voltage - at least 36V
Thank you!
Show Less