Not applicable
Sep 07, 2017
06:28 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
I am building an Arduino-controlled solenoid system designed around the 4x4 Driver Shield from SparkFun based on IRs IPS6044 to drive the solenoids.
I am now spinning my own board and I realised that the driver IC on the shield is now obsolete.
To replace the IPS6044, I chose Infineon's BTS716G. It seems to be very similar to the IPS6044 and is suitable to drive 12 V 0.67 W solenoids.
Is there anything significantly different between the BTS716G and the IPS6044 that I need to consider?
Thank you,
DG
I am now spinning my own board and I realised that the driver IC on the shield is now obsolete.
To replace the IPS6044, I chose Infineon's BTS716G. It seems to be very similar to the IPS6044 and is suitable to drive 12 V 0.67 W solenoids.
Is there anything significantly different between the BTS716G and the IPS6044 that I need to consider?
Thank you,
DG
- Tags:
- IFX
1 Reply

Moderator

Moderator
Mar 29, 2022
12:30 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hello,
BTS716G can be a replacement for AUIPS6044G. Features and performance are similar.
Please do have a check for the power dissipation and thresholds for the inputs and outputs if you are operating close to the limits for AUIPS6044G. There is a slight difference in this.
Thank you
Vishnu Nambrath