Announcements

Join us for FREE at OktoberTech Asia Pacific and hear about decarbonizing future mobility. Click here for more details.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Smart Power Switches Forum Discussions

PriyanshK
Level 1
First question asked Welcome!
Level 1

As STATUS pin of BTT3018EJ is open drain pin, can we connect pull up to 3.3V  in case of Vcc = 5V ?

0 Likes
1 Solution
Meghana
Moderator
Moderator 50 solutions authored 5 likes given 100 replies posted
Moderator

Hello PriyanshK,

Yes. It can be pulled to 3.3V when Vdd=5V. 

STATUS Pin potential should be >2.6V in order to be detected as high by the internal logic when VDD=5V. 

But  if this STATUS pin input is given to an external microcontroller, please also check if the microcontroller is compatible with this potential.

Regards

Meghana 

View solution in original post

0 Likes
1 Reply
Meghana
Moderator
Moderator 50 solutions authored 5 likes given 100 replies posted
Moderator

Hello PriyanshK,

Yes. It can be pulled to 3.3V when Vdd=5V. 

STATUS Pin potential should be >2.6V in order to be detected as high by the internal logic when VDD=5V. 

But  if this STATUS pin input is given to an external microcontroller, please also check if the microcontroller is compatible with this potential.

Regards

Meghana 

0 Likes