Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Has anyone been able to run wiced sense source code with virtual emulator using android studio? Like to know which emulator is being used if you have it running.

0 Likes
1 Solution
Anonymous
Not applicable

Yes I agree.

Plugging in your Device and debugging from there is how our Broadcom developers develop our Apps

Thanks

JT

View solution in original post

4 Replies
Anonymous
Not applicable

I have not used so much AVD (Android Virtual Device). But for sure possible and working

I use most of the time my real device (via USB).

It think all AVD devices should work (you had to create one), e.g. Nexus 5 or 7.
(I have also created one AVD device to simulate my Galaxy S3).

Just to bear in mind that you should select Android versions >= 4.3, best 4.4 (API levels 19 .. 21).


And I do not know what happens with the BLE functions and features. I would assume they are not emulated, most of the stuff related to BLE, e.g. sending Notifications, will not work on AVD (also the counterpart, the WICED Sense, would not be there or connected).
AVD (emulated device) seems to be reasonable for me just for a HW-independent GUI, e.g. if you want to modify the Widgets, the GUI itself. But for BLE features ...?

My suggestion: use Android Studio and debug directly on the target device (e.g. Samsung Galaxy S3, Nexus 7/9). I do it this way, works pretty nice, including breakpoints, stepping through code (with ADB).

Anonymous
Not applicable

Yes I agree.

Plugging in your Device and debugging from there is how our Broadcom developers develop our Apps

Thanks

JT

Anonymous
Not applicable

tjaekel,

Can you let me know the following versions that you are using for Android Studio:

1. Android Studio version:???

I have Android Sudio version 0.8.14

2. JRE version:???

I have JRE 1.8.0_25-b18 x86

3. ADT bundle in SDK: ???

I have adt-bundle-windows-x86-20140702

4. SDK version:???

5. Anything else???

I use windows-7  laptop with 32 bit Operating System which has Intel i7 processor running at 2.8GHz.

With the above version, I am having problem to install necessary components when I try to use AVD. I also tried physically connecting my phone to USB/PC but no success yet to get the project to communicate with my phone.

Nilesh

0 Likes
Anonymous
Not applicable

I use:

1. Android Studio version:

Android Studio version 0.8.14 - the same (beta)

2. JRE version: - I think you need JDK (not just runtime environment JRE)

JDK1.8.0_25

3. ADT bundle in SDK:

adt-bundle-windows-x86_64-20140702

4. SDK version:

Android SDK Manger, Revision 23.0.5

5. Anything else:
NDK: android-ndk-r10c (I think I need for RADStudio only, the C-code support for Android)

apache-ant-1.9.4-bin (might be needed for some other applications, e.g. RADStudio)

AVD Manager:Android SDK Manger, Revision 23.0.5

I run Windows 7 Home, 64bit

Android Studio Tips and Tricks | Android Developers

Managing Virtual Devices | Android Developers

Creating an Android Virtual Device (AVD) in Android Studio - Techotopia