I have set blecm_setmaxconnection(6) so it should be possible to connect 6 devices.

But at the moment I can only connect 3 devices. If I press the button to allow a new connection,

the client is rebooting.

As another test, I set the max connections to 4, but I can sill only connect 3 devices.

The 4. device won't connect to the client.

I appended the traces of both tests.

(The logs are of the hello_client, but the name of it is sensor, so don't get confused 🙂 )

Perhaps somebody has a hint for me what I could check to connect my 6 devices.

One thing I noticed is the numbering of the handles.

The handles are: 0x40, 0x42, 0x43. But where is 0x41 (reserved for the smartphone)?

Also the last device get disconnected with reason 0x3E, but reconnects successfully.

Could this be the reason for the one missing connection if max connections is 4?

0 Likes
1 Solution
Anonymous
Not applicable

Hello Matthias,

I believe we have only tried 8 devices without sending ADV.

JT

View solution in original post

0 Likes
12 Replies
Anonymous
Not applicable

Hello Matthias,

Have you seen this thread?

Re: hello-client switch to slaves after smartphone connectes (con't)

Thanks

JT

0 Likes
Anonymous
Not applicable

Hi JT,

Yes I know the other thread. I know it should be possible to connect 6 sensor to the hello_client.

But my client is rebooting if I'm connecting 4 devices.

0 Likes

Our AE Arvind had provided a fix to this. Let us know if it helps.

How many connect several Max about 20737s?

0 Likes
Anonymous
Not applicable

Hi boont,

Thanks, the link helped a lot.

I added the blecm_setmaxconnection to create insted the INIT function.

But are the max connections I set with that function including the connection to a smartphone?

If I set maxconnection to 6, I'm able to connect to 5 slaves.

So if I want to try to connect to 8 slaves I have to call blecm_setmaxconnection(9)?

0 Likes
Anonymous
Not applicable

Yes. Max number of connections are for both masters and slaves.

So your smartphone which I assume is connected as a master will be considered as one of the connections in hello_client.

However, I'm not sure about the maximum number of connections limited by our hardware and stack implementation,

meaning I'm not sure if you can connect 9 devices.

We'll get back to you on that after asking the developers.

Thank you.

James

0 Likes
Anonymous
Not applicable

Hello Matthias,

So if I want to try to connect to 8 slaves I have to call blecm_setmaxconnection(9)?

1.  The ble_setmaxconnection() needs to be called in the APPLICATION_INIT() function.  If it is done later, then you will have an undefined behavior.

2.  You also need to check how much FREE RAM you have.

3.  For every connection, you need about 800 bytes.

4.  So if you set it to 8 devices, the you will take up 6.4K

5.  The default number of devices is 4, so your RAM usage will go up be 3.2K

6.  Therefore, you need to make sure you are NOT running out of RAM.

Hope this helps

JT

0 Likes
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

Hi JT,

I did further tests.

I removed the setmaxconnections to test if the controller also reboots if it connects to 4 (3) devices at the same time.

There is a log showing you rebooting the controller while connecting to the first device.

After the reboot the devices can connect fine.

I also add code to print the free RAM. But this don't change over the time.

0 Likes
Anonymous
Not applicable

I updated my SDK now and using WICED 2.2.2.

It seems like connecting 7 devices (without smartphone) is no problem anymore.

But if I configure my client to connect to 9 devices (setMaxconn(9)),

I can't connect to one of my devices (the same 7 devices sending ADVs)

The client receives ADV, but a call of blecen_Conn has no effect.

Is there something I can do to connect 8 devices (without smartphone)?

0 Likes
Anonymous
Not applicable

Hello Matthias,

1.  The setMaxconn(9) will not work - you need to set setMaxconn(8).

2.  For every connection, you need about 800 bytes.

Thanks

JT

0 Likes
Anonymous
Not applicable

Hi JT,

Thank you for the clarification.

I thought i had read somewhere I can connect 8 devices and can connect to a smartphone.

This means I have to decide to connect 7 devices and sending ADV or connect 8 devices without sending ADV?

0 Likes
Anonymous
Not applicable

Hello Matthias,

I believe we have only tried 8 devices without sending ADV.

JT

0 Likes
Anonymous
Not applicable

a piconet can include 8 units at the most.,you can refer to the BLE specification 4.0 OR 4.1 .

0 Likes