In SDK 2.0.1, the i2c_temperature_sensor sample using cfa_bsc_OpExtended within its temperature_sensor_write_16_bit_register function.
1. if I right-click the function call cfa_bsc_OpExtended and select "Declarations", I don't find any. By searching these forums I found that this is declared in cfa/cfa.h.
2. in the API documentation, "cfa" isn't mentioned, but I2C is. And there's a i2cm_comboWrite function which would appear to do thse same thing as cfa_bsc_OpExtended.
Is cfa_bsc_OpExtended older API, and the sample hasn't been updated?
Is i2cm_comboWrite to be preferred?
Are there situations where one has to use cfa_bsc_whatever?
Why doesn't a search for "Declarations" on cfa_bsc_OpExtended turn up any results?
thanks.
Solved! Go to Solution.
Hello Stuart,
We just released our latest SDK 2.1.0: WICED Smart Documents & Downloads
Let us know if you find these same issues and I will let the Developers
Thanks
JT
The WICED SMART HW Interfaces Guide here: WICED™ Smart Hardware Interfaces
States that the description of the I2C API is available in WICED-Smart-SDK/Wiced-Smart/cfa/cfa.h
//------------------------------------------------------------------------------
// 10.9.2 Interface Functions
//------------------------------------------------------------------------------
void cfa_bsc_Configure(UINT8 newConfig);
// To configure the I2C serial interface. The configuration values include:
// - Clock Rate
// - Clock divider
// - Delay disable
// - Deglitch disable
CFA_BSC_STATUS cfa_bsc_OpExtended(UINT8* buf,
UINT16 bufCount,
UINT8* addr,
UINT8 addrCount,
UINT8 slaveAdr,
UINT8 operation);
// This function performs blocking read/writes, both addressed and unaddressed
// The amount of data read/written can exceed 8. The address is assumed to be in
// big endian format.
// Input:
// - Pointer to data buffer. For reads, this is where data will be read into
// For writes, data will be written from here.
// - Number of bytes to read/write from the buffer.
// - Pointer to address. Only valid if address count is non-zero; if address count is
// zero, it must be set to 0. This is the address that is sent to the device
// before the operation. In the case of a read, the address is written followed
// by a read. For a write, the address is written, followed by the data.
// The address is assumed to be in big endian format. This is pertinent only
// if the operation requires multiple hardware operations to complete; otherwise
// it is of no significance. The maximum number of bytes that can be read
// in a single hardware transaction is 8 and the maximum that can be written
// is 8 - address size. Note that the address will be modified
// - Number of address bytes. If this is zero, no address is written before the
// operation. If non-zero, the address is written before the read/write. In
// case of a write, the size of the address plus the size of the data must be <= 8
// - Slave address
// - Operation (read/write)
#endif
Hello Stuart
Does this answer your question?
Thanks
JT
JT,
thanks for the pointer to the documentation for cfa_bsc_OpExtended. Perhaps my statement
in the API documentation, "cfa" isn't mentioned
was confusing. The "API documentation" I was referring to there was the HTML documentation at Components/Peripheral Drivers/I2C, which documents routines i2cm_*, which nobody appears to use, and don't seem to work.
But no, it really doesn't answer the four questions I posed.
Hello Stuart,
We just released our latest SDK 2.1.0: WICED Smart Documents & Downloads
Let us know if you find these same issues and I will let the Developers
Thanks
JT