Smart Bluetooth Forum Discussions
text.format{('custom.tabs.no.results')}
As a continuation to this thread: Re: bleprofile_notifyAdvPacketTransmissions doesn't work.
I'm using SDK 2.2.1 and "advertisement_packet_transmission" is not called in some of my programs.
Seems like some bugs are still inside "bleprofile_notifyAdvPacketTransmissions"
After this line of code is executed, the behavior of my WICED Sense will become weird for the next few downloads and become so difficult to get paired.
Show LessHi all,
I have a custom board withe the BLE connected to an external flash memory on following pins:
P3 as CLK
P4 as MOSI
P25 as MISO
P32 as Chip Select
In spiffydriver.h there is no combination for those pins, does it mean that I can't use them? Or is it possible to add the following line:
MASTER2_P03_CLK_P04_MOSI_P25_MISO = 0x00030419,
in Spi2MasterGpioConfigType.
I'm trying to follow the example spi_pressure_sensor, I send only one command (after the initialization of SPIFFY2) to the flash to read it's ID but on the Logic Analyzer I can't see anything.
Any idea?
Thanks
Show LessHello, I trying to find a way to connect only with any wiced sense devices. I want to eliminate the process of selecting the device through the devicepicker activity. Any kind of help is appreciated.
Show LessHi
My device fail to go into deep sleep mode after wake up from deepsleep by a GPIO interrupt and never go into deepsleep mode successfull at the second time.
Regards!
Show LessHi I'm new in using WICED Sense sensor tag. And I'm trying to hard-code a MAC address of a particular WICED sensor tag and connect only to this sensor tag when it is available. Thus, eliminating the need for searching other Bluetooth devices. So, I want to know where to start looking in the code. Any kind of help is appreciated.
Show LessHi all,
I have 4 custom boards. One is master base on Hello_client. The others are slave base on Hello_sensor.
I try to send write command to all hello_sensor. I use the API like this:
bleprofile_sendWriteCmd(handle, data, data_size);
But only one slave can receive the command packet.
What is the method can send packet to all slave?
Show LessIs there an off-the-shelf socket that is available from Broadcom or some other entity that can be designed into a board/fixture (in conjunction with a TAG3 board) for the purpose of creating a custom programmer for a small number of the BCM20736S modules?
Although we have testpoints on our PCB for programming it, there is a need for a small number (~50) of the chips to be programmed before PCB assembly.
Thanks,
David Smith
Show LessIn the process of moving our design from prototype to production, we were directed to a source for an off-the-shelf programmer for the BCM20736S module. This is something that we've been periodically searching for and something that I imagine a number of other users have been seeking as-well.
The manufacturer of the programmer is BP Microsystems. Their socket adapter for the BCM20736S is the ASMC48LGD or the FX4ASMC48LGD. This socket must be paired with one of their programmers to be a fully functional programming solution. However, the socket alone may be of use to those that need a physical interface to the chip but will be creating their own programming back-end (possibly using the TAG3).
Link to ASMC48LGD page:
http://www3.bpmicro.com/DeviceList.nsf/SocketSolutions/ASMC48LGD
Link to FX4ASMC48LGD page:
http://www3.bpmicro.com/DeviceList.nsf/SocketSolutions/FX4ASMC48LGD
This information is provided as-is for the benefit of others; however, keep in mind that we have not used their programmer or socket and we have not vetted it in any way.
Regards,
David
Show LessNow I can download the app either in EEPROM or spi flash use the SDK,however ,here comes the question that the SDK has set the SPI1 or IIC as the interface,Our product want to set the SPI2 as the interface,I know I need to reconfig the SDK environment,but I did't find where to config the GPIO definition and SPI2,do you have any ideas?
Show Less