Smart Bluetooth Forum Discussions
Sort by:
Smart Bluetooth
how to speed up download
Solved
Downloading app takes 30-60 seconds at 115200 baud. Why so slow?Is debug info (symbols, etc.) include, which can be disabled?Is the compilation code-...
Show More
Downloading app takes 30-60 seconds at 115200 baud. Why so slow?Is debug info (symbols, etc.) include, which can be disabled?Is the compilation code-space optimized?Thanks.
Show Less
Smart Bluetooth
Hi Sir, Can I use SDK 1.0.1 to support client & server mode with two BCM20732 application? Ex1. BCM20732(Client) <--Pairing-> BCM20732(HR pro...
Show More
Hi Sir, Can I use SDK 1.0.1 to support client & server mode with two BCM20732 application? Ex1. BCM20732(Client) <--Pairing-> BCM20732(HR profile server) Ex2. BCM20732(Client) <--Pairing-> BCM20732(HR profile server) <-Pairing--> BCM20732(Proximity profile server) <-Pairing--> how many server can be support ? Ex3. BCM20732(Client) <--Pairing-> BCM20732(HR + Findme + Proximity profile server) Should I refer which sample code ? thanks a lot.
Show Less
Smart Bluetooth
Bcm920732eval_q32
Solved
Can I use BCM920732EVAL_Q32 instead of BCM920732TAG-00 with WICED Smart SDK?Id like to know how to program an application into it by the IDE.
Show More
Can I use BCM920732EVAL_Q32 instead of BCM920732TAG-00 with WICED Smart SDK?Id like to know how to program an application into it by the IDE.
Show Less
Smart Bluetooth
appFineTimer
Solved
When I set 1500 as fine_timer_interval of BLE_PROFILE_CFG, appFineTimerCb is called every 1 sec.Is 1000 maximum value for this timer?I have another qu...
Show More
When I set 1500 as fine_timer_interval of BLE_PROFILE_CFG, appFineTimerCb is called every 1 sec.
Is 1000 maximum value for this timer?
I have another question.
The difference between normal timer and fine timer is only resolution.
Is my understanding correct?
Id like to have detailed API documents.
Show Less
Smart Bluetooth
Hi Team, I found a issue by disabling "powersave_timeout" mode. Is any setting config which i miss ? thanks a lot. Disable "powersave_time...
Show More
Hi Team, I found a issue by disabling "powersave_timeout" mode. Is any setting config which i miss ? thanks a lot.
Disable "powersave_timeout" modeThere are one strange issue about Show Less
Smart Bluetooth
Smart Bluetooth
Question: Why do I get an error dialog box stating "C:Program FilesWIDCOMMBluetooth SoftwareBTWLeApi.Dll" when running the HelloClient.exe demo appli...
Show More
Question: Why do I get an error dialog box stating "C:Program FilesWIDCOMMBluetooth SoftwareBTWLeApi.Dll" when running the HelloClient.exe demo application?Note: After clicking the OK button on the dialog box, another error dialog box is shown stating the Broadcom Bluetooth profile pack for Windows (BTW) has to be installed. It can be closed/ignored.
Show Less
Smart Bluetooth
Question: The size of the 20732 peripheral UART (receiver) FIFO is 16 bytes. Can it be increased?Answer: No. The size is limited by the hardware and...
Show More
Question: The size of the 20732 peripheral UART (receiver) FIFO is 16 bytes. Can it be increased?Answer: No. The size is limited by the hardware and cannot be increased.
Show Less
Smart Bluetooth
What is HelloClient.exe? How do I compile it?WICED-Smart customers experimenting with the Broadcom WICED-Smart evaluation board (BCM920732TAG_Q32) wi...
Show More
What is HelloClient.exe? How do I compile it?WICED-Smart customers experimenting with the Broadcom WICED-Smart evaluation board (BCM920732TAG_Q32) will want to see the SDK in action (e.g. compile, launch, test an application). A good vehicle to verify proper SDK installation and hardware functionality is shown in the Wiced-Smart Quick Start Guide -- Found in SDK folder ~Doc/WICED-Smart-QSG as a .pdf file. Those directions reference the Helloclient.exe demo application found within the ~WICED-Smart-SDK/Apps/RAM/hello_sensor/HelloClient folder.The 32-bit and 64-bit versions of HelloClient.exe for Windows come pre-compiled with the SDK installation, but if you want to modify it for yourself:1. Run Visual Studio 2012 or equivalent. Open project WICED-Smart-SDKAppsRAMhello_sensorHelloClientWindowsHelloClient.vcxproj2. In the file HelloClient.cpp, replace the line #include "C:BTW6.5.1Windowsinclude twleapis.h" by the line #include "btwleapis.h"3. Create
Show Less
Smart Bluetooth
Hi,I had installed WICED-Smart-SDK-1.0.1-IDE-Installer.exe, now I can use eclipse to build and download application by HCI uart port.I have jlink debu...
Show More
Hi,
I had installed WICED-Smart-SDK-1.0.1-IDE-Installer.exe, now I can use eclipse to build and download application by HCI uart port.
I have jlink debugger on my hand, can I use jlink to in circuit debug WICED Apps when run eclipse? Do you have corresponding proposal for user?
BR
Kai Ren
Show Less