Smart Bluetooth Forum Discussions
In general, the device's name is defined in the field "local_name" of the data structure BLE_PROFILE_CFG and launched by the function "bleapp_set_cfg".
If I will identify the different device's name in the same firmware, how to change the device's name by function call?
Thanks!
Jack Huang
Show LessIs there any recommendation provided by Broadcom for the SW that should be used to pass the FCC certification for the BCM20736S?
Is there a Test Suite that will be provided by Broadcom that can be used during the FCC certification work? Something that would cover BLE stress test or specific scenarios?
Is this possible to develop DLL file for VB.NET or VC# based on your API and your C++ samples? Do you know anyone who has done that?
Thanks,
John
Show LessHi Broadcom,
I can't find stock anywhere for your BCM20737 part. I can't even find a datasheet for the part.
I am building a board for a customer and need help ASAP.
Please help.
Thank You,
John.
Show LessHello,
I'm just getting started on using the WICED Smart dev kit. I've read all of the documentation I could find (Quickstart Guide - QSG201-R, Hardware User Manual - HWUM100-R, Harware Interfaces - AN101-R, etc.) and I'm still confused about how to use the DIP switch SW4. What are the different settings possible? When would I use the application mode instead of the HCI_UART mode?
Any help would be much appreciated. Thank you
Show LessI am just starting a discussion on BT (LE) protocol analyzer/sniffer. Could you please share your experience with some of the equipment out there that you are using regularly to analyze a BT transmission? Also it would be helpful to put the pros/cons of the equipment/solution with a bit of your experience.
Show LessHi all,
The specification for the BCM20732 lists the Receiver RF Maximum input @-10dBm. This is a pretty low value. What would be the max "Maximum input" value? I am looking at the maximum power the chipset can take without being destroyed. This is not in the datasheet currently and I am wondering if someone can share some values.
Thanks,
Show LessHi, I'm brand new to WICED-Smart and I'm diving into the SDK, but I can't seem to find where the main thread begins. Could someone please point me in the right direction?
Show LessHi, I'm facing a strange problem, an need someone's advise.
I made a board using 20732S, keep button 1 and PUART schematic same as demo board.
Test with hello sensor code, and button interrupt 1 works. debug trace log can be shown to HCI UART, but cannot show to PUART,
where I've modified "spar_init.c" for controlling log output correctly.
When I configure output to PUART, I found I have to press button 1 for 2 times, then PUART can output. The message can output until the button pressed twice, after that it output the log normally.
Is there any suggestion for this issue? Thank you in advanced.
Show Less