Smart Bluetooth Forum Discussions
Dear Team
I would like to ask you to check a possibility regarding tuning the advertisement channel, For example, they will be corresponded with an each channel as follow, also they will be used for the BLE scanning activity for each channel.
1st BLE chipset tune for 37 advertisement channel.
2nd BLE chipset tune for 38 advertisement channel.
3rd BLE chipset tune for 39 advertisement channel.
Would you please help the possibility?
Thank you
Daniel
Show Less
Hi Sir,
I have a question. When I start transferring the upgrade data, it seems that the data keep transmitting without ack from device.
If I want to do the rate control and want an ack when device get the data, can I change the property like the HANDLE_WS_UPGRADE_CHARACTERISTIC_CONTROL_POINT?
Show Less
Hey guys,
I have to program a communication interface between a sensor and a microcontroller. The two participants of the communication are an accelerometer (ADXL363) and the BCM20736S and for the communication I chose the SPI of the BCM.
The programming tool "Wiced Smart SDK" provides some SPI-examples but I don't understand everything.
So, I have some questions which won't be the last but the first questions I had
Do I have to send the address of the register and the value I want to write in it at the same time? Or are these two seperate steps?
And how do I have to configure the GPIOs?
I work with the Anaren's Atmosphere System.
Thanks for your help!
André
Show LessI have been able to create a make target following the recovering steps from the blog.
The download process completes successfully; however, I can no longer connect to my phone.
Upon connecting the battery, the kit is detectable for a few seconds. That is, I can see its name when the android app is searching.
However, it does not pair nor communicates in any other way.
The LED, rather than slowly pulse, it stays bright red.
Any ideas?
Thank you
-Kevin RR
Show LessI have recently received Wiced Sense Kit but I am trying to use it in advertisement mode so any app can received the advertisement and inform the server about the presence of the device. Appreciate your help on this
Show LessMy CPE/Gateway is with BCM47081A0, How can I make IoT protocol enabled, for example Axeda Platform...?
Dear All,
I am using WICED SmartIDE 1.1 with BCM20732 to develop an application.
I have encountered a problem now.
The connection between always disconnect by slave during encryption stage.
Attached file is the sniffer trace.
Could anyone give me some suggestions?
my developing enviroment are as below:
SDK:WINCED Smart 1.1
Master:
iphone 4S
ios:7.1.2
Slave:
cpu:BCM20732
Thanks.
Show LessWe can see on the table 2 in page 13 of BCM20732S Technical Reference, that this pin's alternative function support "Peripheral UART TX(PUART_RX)".
But I guess this should be "Peripheral UART TX(PUART_TX)" or "Peripheral UART RX(PUART_RX)" . This this something typo? Which of TX or RX is correct?
Show LessI am trying to advertise the following data
adv[0].len = 16+1;
adv[0].val = ADV_SERVICE_UUID128_COMP; // (AD_TYPE == 0x07)
BT_MEMCPY(&adv[0].data, vendor_service_uuid, 16);
adv[1].len = 10+1;
adv[1].val = ADV_LOCAL_NAME_COMP;
BT_MEMCPY(&adv[1].data[0], local_name, 10);
adv[2].len = 1+1;
adv[2].val = ADV_MANUFACTURER_DATA; // (AD_TYPE == 0xff)
adv[2].data[0] = variable & 0xFF;
But it only advertises ADV_SERVICE_UUID128_COMP and ADV_LOCAL_NAME_COMP, I can not see the manufacturing data.
The total length here is 17+11+2 = 30 bytes.
Any suggestion on why I can't see the manufacturing data?
Show Less