Smart Bluetooth Forum Discussions
Hi,
I would like to change the MAC address to a desired value in the "....._create()" function.
Is there a "set" MAC address command similar to the one that "gets" the MAC address (emconinfo_getAddr())?
I was hoping there would be something with a prototype like "bool emconinfo_setAddr(UINT8* str);" or anything similar to that.
Could someone help?
Thanks!
Cheers,
Gil
Show LessSince the TAG2 board does not have the actual module populated on it, how could one best compare the performance of the module vs other BLE solutions? Is there a ref design or Eval board specifically tailored for the module? Since environmental factors like plastic housing, proximity to body in wearable applications can influence the performance of frequency shift and general RF performance it would be useful to have a hardware platform to evaluate...
Show LessAs title, Is there any API to use Watchdog on SDK 1.1?
I found some APIs in bleappfwu.h
void restartWatchdog(INT32 checkWatchDog);
void watchdogExpired(UINT32 unused);
But there is no instruction to use. Can somebody help me.
I'm using BCM902732_BLE_KIT and WICED-Smart-SDK-1.1.0.
Thanks.
Show LessHi,
Is TEST UART the only interface that can accept HCI commands for RF testing?
One of our customers is going to use SPI for connection between BCM20736 and their host MCU.
They would like to use SPI to pipe HCI commands from the host MCU to BCM20736.
Thanks,
Wataru Sugimoto
Show LessHow many volt (at VBAT) is the voltage condition of the attached current consumption table for BCM20737S?
And the sleep current 12uA (nominal) is correct??
[20737S-DS100-R.pdf] page 13
Additionally, the above one [20737S-DS100-R.pdf] and the following document [WICED-Smart-DG100-R.pdf] has huge difference regarding sleep current. Which is correct for BCM20737S?
OR, WICED-Smart-DG100-R.pdf table 2 is not for BCM20737S?
I always confused about current consumption because BCM20737 related documents seem fragmented.
Please correct and keep it updated if the current data sheet (20737S-DS100-R.pdf) is obsoleted otherwise everyone must be confused.
[WICED-Smart-DG100-R.pdf] page 12
12
Show LessHi,
I read this important function about devices BCM20736/7 " Support for Wireless Charging".
Please, could send me more info, doc and applications notes.
Thanks a lot
Pierluigi
Show LessHi,
Has anyone been successful in enable the debug traces ?
There is a procedure description for the BCM92073TAG. However I have not found information about how to do it for the WICED Sense.
Thanks for any hint !
Cheers,
Benoit.
Show LessHello
We are looking at an application where a BLE Tag is able to perform the following functions
a) Send BLE Advertisement data
b) Scan for BLE advertisements from other tags
c) Store scan information locally and send scan information to an iOS / Android app whenever the iOS/Android device is reachable
We are exploring different chipset options. Can anyone guide me on if the Broadcom WICED family of modules will be the right modules to support the above use cases
Best
Prasanna
Show LessHi Guys,
I have purchased ACKme's AMS001-E01 ‘Wahoo’ and would like to create my own Firmware using WICED.
Is it possible to get Platform Files for this board so I can add it as a make Target in the WICED IDE.
Is it possible to use the source Files from WICED SDK as a basis for my own firmware on AMS wahoo Eval board ?
Many Thanks in Advance,
Ruben Mayer
Show Less