Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Smart Bluetooth Forum Discussions

Anonymous
Not applicable

Hi

I am trying to make a firmware for the WICED sense tag that only adv. when one of the buttons on the side is pressed. I have used the wizard to generate code that supports 'button' only. However the method 'access_tag_interrupt_handler' is only called when pressing the button and not when the button is depressed. Another thing is that the method is only called when pressing the lower button (named 'App Button') and not the top button (named 'Wake Button').

This bring me down to the two questions:

1. How can I get the app to react separately on both buttons?

2. How can I get the app to react when one of the buttons is depressed?

0 Likes
1 Solution
Anonymous
Not applicable

Hi thomas_bonde,

Don't know if you still have this problem but I have just created a short demo on using interrupts with with the WICED Sense.  In my video you can see that when I press the bottom button, the LED will flash, once from when I press the button and once for when I release.  In my code as you will see, I put for both both edges.  Similarly, you can register two difference interrupt handlers, one for rising one for falling.  Then in my video, I use the top button to beep the buzzer, again once for pressed and once for depress.

Hope this helps,

Kevin

void ble_tx_create(void){

  bleprofile_GPIOInit(bleprofile_gpio_p_cfg);

    bleprofile_Init(bleprofile_p_cfg);

    gpio_configurePin(0, 0, GPIO_EN_INT_BOTH_EDGE, GPIO_PIN_OUTPUT_LOW);

    gpio_configurePin(0, 4, GPIO_EN_INT_BOTH_EDGE, GPIO_PIN_OUTPUT_LOW);

    //register for interrupts on pins 0 and 4 (push button)

    {

         UINT16 masks1[3] = {(1 << 0), 0 , 0};

         gpio_registerForInterrupt(masks1, interrupt_handler1, 0);

         UINT16 masks2[3] = {(1 << 4), 0 , 0};

         gpio_registerForInterrupt(masks2, interrupt_handler2, 0);

    }

}

void interrupt_handler1(void* parameter, UINT8 arg) {

       bleprofile_LEDBlink (50, 50, 3);

}

void interrupt_handler2(void* parameter, UINT8 arg) {

       bleprofile_BUZBeep(100);

}

Video Link : 1349

View solution in original post

0 Likes
8 Replies
Anonymous
Not applicable

Hello Thomas,

Please use the hello_sensor.c as the appropriate app to start your development.

Some functions of the Smart Designer did not produce code for the buttons

1.  The first button is a Wake Button as the WICED Sense kit explains

2.  The second button can be used as an Application button

3.  Please see the WICED Sense Kit BLOG for further questions.

The Schematics for WICED Sense Kit are located here: WICED Sense Reference Design Schematic (PDF)

Hope this helps

Thanks

JT

0 Likes
Anonymous
Not applicable

Hi JT,

Thank you for your swift reply.

I have now build and downloaded the 'hello sensor' and enabled the trace functionality. However I still cannot get the message for when the 'App Button' is DEpressed?

Here is what I get when the app button is pressed:

17:12:10 - hello_sensor_timeout(INT)But1:1 But2:0 But3:0

17:12:10 - 48 65 6c 6c 6f 20 33 xcheck retCode = 00ADV start high: 000000000000

17:12:10 - XH*handlerj0e 04 01 0a 20 00

17:12:10 - blecm evt handlerj0e 04 01 06 20 00

17:12:10 - blecm evt handler:*04 01 0a 20 00

17:12:11 AppTimer(adv, conn) stopped: 1

17:12:11 BLE_high_un_adv:timer(0)

- nothing happens when I release the button, - just like I saw it in the Smart Designer generated code?

Thanks,

Thomas

0 Likes
BoonT_56
Employee
500 likes received 250 likes received 100 likes received
Employee

I checked out the hello_sensor.c  on my tag3 and I was able to see the below when the sw1 is pressed once:

11:53:00 - hello_sensor_timeout:381

11:53:01 -

11:53:01 - hello_sensor_timeout:382

11:53:01 -

11:53:01 - (INT)But1:1 But2:0 But3:0

11:53:01 -

11:53:01 - 48656c6c6f2031

11:53:01 -

11:53:01 -  permission check retCode = 00

11:53:01 - ADV start high: 000000000000

11:53:01 -

11:53:01 -

11:53:01 - blecm evt handler:

11:53:01 - 0e04010a2000

11:53:01 -

11:53:01 - blecm evt handler:

11:53:01 - 0e0401062000

11:53:01 -

11:53:01 - blecm evt handler:

11:53:01 - 0e04010a2000

11:53:01   AppTimer(adv, conn) stopped: 1

11:53:01   BLE_high_un_adv:timer(0)

11:53:02 - hello_sensor_timeout:383

11:53:03 -

11:53:03 - hello_sensor_timeout:384

11:53:04 -

11:53:04 - hello_sensor_timeout:385

Can you try this out on a tag?

0 Likes
BoonT_56
Employee
500 likes received 250 likes received 100 likes received
Employee

Any luck with your Sense kit?

0 Likes
Anonymous
Not applicable

Hi Boont,

The posted trace messages in my previous response outlines what happens when I press the 'App Button' using the 'hello sensor' source code.

I was of the understanding that I should get a call back to the 'hello_sensor_interrupt_handler method', when i am releasing the 'App Button'. however that might not be the case?

reg.

TB

0 Likes
BoonT_56
Employee
500 likes received 250 likes received 100 likes received
Employee

Are you doing the above on a tag3 or sense board? I know some folks reported here that they can get tracing from the sense board, but it is not officially supported actually.

0 Likes
BoonT_56
Employee
500 likes received 250 likes received 100 likes received
Employee

So have you got a chance to try out on a tag3?

thomas_bonde

0 Likes
Anonymous
Not applicable

Hi thomas_bonde,

Don't know if you still have this problem but I have just created a short demo on using interrupts with with the WICED Sense.  In my video you can see that when I press the bottom button, the LED will flash, once from when I press the button and once for when I release.  In my code as you will see, I put for both both edges.  Similarly, you can register two difference interrupt handlers, one for rising one for falling.  Then in my video, I use the top button to beep the buzzer, again once for pressed and once for depress.

Hope this helps,

Kevin

void ble_tx_create(void){

  bleprofile_GPIOInit(bleprofile_gpio_p_cfg);

    bleprofile_Init(bleprofile_p_cfg);

    gpio_configurePin(0, 0, GPIO_EN_INT_BOTH_EDGE, GPIO_PIN_OUTPUT_LOW);

    gpio_configurePin(0, 4, GPIO_EN_INT_BOTH_EDGE, GPIO_PIN_OUTPUT_LOW);

    //register for interrupts on pins 0 and 4 (push button)

    {

         UINT16 masks1[3] = {(1 << 0), 0 , 0};

         gpio_registerForInterrupt(masks1, interrupt_handler1, 0);

         UINT16 masks2[3] = {(1 << 4), 0 , 0};

         gpio_registerForInterrupt(masks2, interrupt_handler2, 0);

    }

}

void interrupt_handler1(void* parameter, UINT8 arg) {

       bleprofile_LEDBlink (50, 50, 3);

}

void interrupt_handler2(void* parameter, UINT8 arg) {

       bleprofile_BUZBeep(100);

}

Video Link : 1349

0 Likes