- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I designed a mainboard for bcm20732s module which provide VCC and GND for 20732s.
I could download application, like hello_sensor, into 20732s, but after running, trace info like this, why battery level is critical? If battery is low, why download process is ok? SMART SDK is 1.1.0.
GPIO_WP:OFF=0
hello_sensor_create()
1.00
GattDB:20be40, 20bf73
hdl:perm:len:maxlen:uuid
0001:02:02:02:2800
01 18
0014:02:02:02:2800
00 18
0015:02:05:05:2803
02 16 00 00 2a
0016:02:10:10:2a00
48 65 6c 6c 6f 00 00 00 00 00 00 00 00 00 00 00
0017:02:05:05:2803
02 18 00 01 2a
0018:02:02:02:2a01
00 02
0028:02:10:10:2800
23 20 56 7c 05 cf 6e b4 c3 41 77 28 51 82 7e 1b
0029:02:13:13:2803
32 2a 00 26 f6 69 91 68 ee c2 be 44 4d b9 5c 3f
2d c3 8a
002a:82:07:07:00
48 65 6c 6c 6f 20 30
002b:0a:02:02:2902
00 00
002c:02:13:13:2803
0a 2d 00 1a 89 07 4a 2f 3b 7e a6 81 44 3f f9 a8
f2 9b 5e
002d:8e:01:01:00
00
004d:02:02:02:2800
0a 18
004e:02:05:05:2803
02 4f 00 29 2a
004f:02:08:08:2a29
42 72 6f 61 64 63 6f 6d
0050:02:05:05:2803
02 51 00 24 2a
0051:02:08:08:2a24
31 32 33 34 00 00 00 00
0052:02:05:05:2803
02 53 00 23 2a
0053:02:08:08:2a23
93 b8 63 80 5f 9f 91 71
0061:02:02:02:2800
0f 18
0062:02:05:05:2803
02 63 00 19 2a
0063:02:01:01:2a19
64
GattDB complete
02 01 06 06 09 48 65 6c 6c 6f 04 0d 00 00 00 03
03 00 00
02 0a 04
bd_addr: 20732a093e41
GPIO1(11)
GPIO0(104)
GPIO14(1003)
GPIO15(20)
GPIO28(2001)
Interrupt mask:0001 0000 0000
GPIO_WP:OFF=0
GPIO_BUTTON1:OFF=0, INT:1
GPIO_LED:OFF=1
GPIO_BAT
GPIO_BUZ:OFF=0
lebat_bat_lvl_hdl:0063
64
Battery level is critical, Shutting down
permission check retCode = 00
00
Battery level: 0/100
Fine Timer(1000 ms, 1/sec, 80 tick)
Normal Timer(1 s, 80 tick)
23 20 56 7c 05 cf 6e b4 c3 41 77 28 51 82 7e 1b
02 01 05 11 07 23 20 56 7c 05 cf 6e b4 c3 41 77
28 51 82 7e 1b 06 09 48 65 6c 6c 6f
BLE_high_un_adv:timer(1)
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
In your database_init function, your program probably calls blebat_init(). This function actually comprises of four functions (dbinit, config, startmonitoring, pollmonitor), all which are loaded in ROM.
If you want just the message to go away, you can just comment out startmonitoring and pollmonitor.