- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
When I open WsOtaUpgrade.exe, a error message occur: "Failed to open the patch file." What's wrong with that?
I can open HelloClient application.
Solved! Go to Solution.

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Once the download is successful, the device will automatically boot into the new application image.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
How about drop the FW file(patch) into the application?
Or specifying file name on Command Prompt may work.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
I do ota test as below:
1. download "RAM.ota_firmware_upgrade-BCM920732TAG_Q32 download" into my bcm920732_tag.
2. use command prompt to open WsOtaUpgrade.exe with "hello_sensor-BCM920732TAG_Q32-rom-ram-Wiced-release.ota.bin"
3. I can see above picture and click start.
4. Then, ota processing is finished, then click "Done".
If hello_sensor-BCM920732TAG_Q32-rom-ram-Wiced-release.ota.bin was running, I can see ble trace message from prm_uart, but the result is nothing at all.
So, when ota is finished, how can user trigger the application running in bcm920732_tag?

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Once the download is successful, the device will automatically boot into the new application image.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
I use bcm20732tag and sdk is wiced smart v1.1.0, try it again.
Upgrade is ok and I can see "Success" on the PC's utility, but new application didn't run automation_io-BCM920732TAG_Q32-rom-ram-Wiced-release.ota.bin because I had upgrade it by ota.
I can captured trace information through com port, this is detail when upgrade process began.
hello_sensor_timeout:347
hello_sensor_timeout:348
hello_sensor_timeout:349
hello_sensor_write_handler: handle ff03
hello_sensor_write_handler: handle ff02
Command:1 State:0
send_status 0
hello_sensor_write_handler: handle ff02
Command:2 State:1
Active: 0x000004C0, Upgrade: 0x00008000, UG length: 0x00007B00
state:2 total_len:21022
send_status 0
a2 1a 00 6c 30 00 00 1b 33 00 00 00 00 00 00 14
1e 08 02 b0 04 00 00 00 00 00 00 00 00 72
hello_sensor_timeout:350
hello_sensor_timeout:351
hello_sensor_timeout:352
hello_sensor_timeout:353
hello_sensor_timeout:354
hello_sensor_timeout:355
hello_sensor_timeout:356
hello_sensor_timeout:357
hello_sensor_timeout:358
hello_sensor_timeout:359
hello_sensor_timeout:360
hello_sensor_timeout:361
hello_sensor_timeout:362
hello_sensor_timeout:363
hello_sensor_timeout:364
hello_sensor_timeout:365
hello_sensor_timeout:366
hello_sensor_timeout:367
hello_sensor_timeout:368
hello_sensor_timeout:369
hello_sensor_timeout:370
hello_sensor_timeout:371
hello_sensor_timeout:372
hello_sensor_timeout:373
hello_sensor_timeout:374
hello_sensor_write_handler: handle ff02
Command:3 State:2
ws_verify rcvd:e10a4d4f calculated:e10a4d4f
send_status 0
hello_sensor_timeout:375
a2 1a 00 6c 30 00 00 1b 33 00 00 00 00 00 00 14
1e 08 02 b0 04 00 00 00 00 00 00 00 00 72 06 00
0b 00 00 00 00 01 b3 01
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
When ota downloading was finished, not only application didn't run, but also I couldn't download application through hci interface which is traditional way for upgrade.
The only way was to recover this tag, then everything was ok.

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
OTA/uart upgrade divides the EEPROM into roughly two halves as in one of the comments in ws_upgrade.c, and if you look at this layout, it requires an EEPROM larger than 32Kbytes. The 20732 tag board comes with only a 32kbyte EEPROM, which is not enough to store two images (for fail-safe upgrade) and the EEPROM silently wraps around to the lower addresses and so corrupting the image. So use a larger EEPROM (64Kbytes) and it should work for you.
The newer 20736 and 20737 tag boards have 64Kbyte EEPROMs, so you will not have this problem with these tags (and SDK 2.0).
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
If I use bcm20732s module, can it be solved?
I know that bcm20732s embed an eeprom which is 512kb, 64kB.

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Yes, the 20732S modules (S03 version that is shipping now) has a 64kbyte EEPROM and updates should wok with it.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
I've replace from 32Kbyte to 64Kbyte EEPROM but It is not working.
Plz,Let me know how to upgrade using EEPROM
1) ws_upgrade_verify() return value is ture after ota.bin was downloaded to EEPROM
2) 20732 is not working
condition>I can't change SDK 2.0. I have to use SDK 1.1.0.
1) const WS_UPGRADE_NV_LOC_LEN nv_loc_len[2] =
{
{
/* .ss_loc = */ {0, 256},
/* .ds1_loc = */ 0x4C0, // ConfigDSLocation
/* .ds1_len = */ 0x7B00, // ~31KB
/* .ds2_loc = */ 0x8000,
/* .ds2_len = */ 0x7B00, // ~31KB
/* .vs1_loc = */ 0x140, // DLConfigVSLocation
/* .vs1_len = */ 0x200, // DLConfigVSLength
/* .vs2_loc = */ 0, // No VS2 for EEPROMS
/* .vs2_len = */ 0 // No VS2 for EEPROMS
},
2) 20732_EEPROM.btp
DLConfigSerialControlBaudRate = 115200
DLConfigEEPROMAccessSpeed = 100
DLConfigVSOffset = 0
ConfigDSLocation = 1216
DLConfigSSLocation = 0
DLConfigIncludeBTWSecurityKey = 0
DLConfigVSLocation = 320
DLConfigVSLength = 512
DLConfigRemoteDeviceCount = 0
DLConfigBD_ADDRBase = "20732A0*****"
DLConfigFixedBD_ADDRFlag = "Can change"
OTAFWUAckAllRecords = 0
OTAFWUUpdateFirmware = 1
OTAFWUUpdateConfig =
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
This problem is cleared. I have wrong binary file
Thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi Sir,
May I ask what's the os you run for this application? Win7 or Win8?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
I have the same error,When I open WsOtaUpgrade.exe, a error message occur: "Failed to open the patch file."
how do you fix it?

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
I created a new thread for this here: Why error occur when I open WsOtaUpgrade.exe?