Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
SuLe_1710756
Level 5
Level 5
10 likes received First like received First like given

Hi maxsong,

Our customer is considering to use serial flash to store user data. Could you confirm if customer is possible to use part number like attached files?

Thanks,

Sung-Mok

0 Likes
1 Solution
Anonymous
Not applicable

Hello Sung-Mok Lee,

Our SFLASH Drivers follow the command set of the Macronix Serial FLASH:

MX25U4033EM1I-12G.

From their manual:

http://www.macronix.com/Lists/DataSheet/Attachments/2641/MX25U4033E,%201.8V,%204Mb,%20v1.8.pdf

You have to make sure you can follow this command structure.

pastedImage_0.png

Thanks

JT

View solution in original post

0 Likes
3 Replies
Anonymous
Not applicable
0 Likes
MichaelF_56
Moderator
Moderator
Moderator
250 sign-ins 25 comments on blog 10 comments on blog

sung-mok_lee

Per maxsong's request, I will ask the Applications team to check with the developers next week to determine if the MX25V1006E, 2.5V, 1Mb or EN25F10A-104XIP can be used as alternate NVRAM choices on your SoC design (on the SiP module, NVRAM in internal and cannot be modified).

More to follow next week.

lucyli j.t

0 Likes
Anonymous
Not applicable

Hello Sung-Mok Lee,

Our SFLASH Drivers follow the command set of the Macronix Serial FLASH:

MX25U4033EM1I-12G.

From their manual:

http://www.macronix.com/Lists/DataSheet/Attachments/2641/MX25U4033E,%201.8V,%204Mb,%20v1.8.pdf

You have to make sure you can follow this command structure.

pastedImage_0.png

Thanks

JT

0 Likes