- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Here are a few common tips and tricks when beginning SDK 2.1.1 development:
Java JRE Error:
The WICED SMART SDK utilizes a 32-bit version of an Eclipse based IDE which requires a 32-bit version of JRE to be installed.
If you have the 64-bit JRE installed you will need to install the 32-bit version as well.
The JRE is designed to allow both 32 and 64 bit variants to be installed on the same system.
Error on Download:
**** Build of configuration Release for project WICED-Smart-SDK ****
/Users/JT/Documents/WICED/WICED-Smart-SDK-2.1.1/WICED-Smart-SDK/make wiced_sense-BCM920737TAG_Q32 download
Linking target ELF
OK, made elf.
Call to wiced_sense_spar_crt_setup @ 002079a1
OK, made /Users/JT/Documents/WICED/WICED-Smart-SDK-2.1.1/WICED-Smart-SDK/Wiced-Smart/spar/../../build/wiced_sense-BCM920737TAG_Q32-rom-ram-Wiced-release/A_20737A1-wiced_sense-rom-ram-spar.cgs. MD5 sum is:
d2d93699236ab6dbcf0ed18e0720c22b ../../build/wiced_sense-BCM920737TAG_Q32-rom-ram-Wiced-release/A_20737A1-wiced_sense-rom-ram-spar.cgs
--------------------------------------------------------------------------------
Patches start at 0x00204568 (RAM address)
Patches end at 0x002052D0 (RAM address)
Application starts at 0x00204F70 (RAM address)
Application ends at 0x0020797E (RAM address)
Patch size (including reused RAM) 3432 bytes
Patch size 2568 bytes
Application size 10766 bytes
------
Total RAM footprint 13334 bytes (13.0kiB)
--------------------------------------------------------------------------------
Converting CGS to HEX...
Conversion complete
Creating OTA images...
Conversion complete
OTA image footprint in NV is 12829 bytes
Detecting device...
+------------------------------------------------------------------------------------------+
| No BCM20737 detected |
| 1. Verify the BCM20737 tag is connected _AND_ powered |
| 2. Verify SW2 and SW3 switches are towards Vusb and Vreg respectively and all SW4 |
| switches are set to ON |
| 3. Press the reset button on the tag and retry |
| |
| If this problem persists, the EEPROM on the tag may be corrupted |
| Please see Appendix D in the Quick Start Guide for recovery instructions |
+------------------------------------------------------------------------------------------+
Download failed. This version of the SDK only supports download to BCM20736A1 and BCM20737A1 devices
If this happens, 2 things might be wrong:
- You may NOT have installed the Silicon Drivers:
- The WICED Sense Kit is NOT in download mode so:
- Hold the External WAKE Button (1) down for 3 seconds and try to download again.
More Tips and Tricks to come
JT
Solved! Go to Solution.
- Labels:
-
WICED Sense
- Tags:
- tips and tricks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi All,
Here is the procedure I hqve followed with success to download q build :
0- update the usb driver
1- remove the battery
2- connect to the usb cable
3- place the battery and remove it
4- build and download
=> application is up and running. No need to open the box.
Cheers,
Benoit.