Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

When uart receives bytes, it does go entering to interrupt call back often.

I should send uart packet several times (2 ~ 8), then uart can receive.

Byte size is regardless.

Can anybody have same experiences?

int Uart_Init(BLE_PROFILE_PUART_CFG *puart_cfg, BLECM_FUNC_WITH_PARAM puart_rx_callback)

{

puart_selectUartPads(puart_cfg->rxpin, puart_cfg->txpin, 0x00, 0x00);


// Initialize the peripheral uart driver

puart_init();

// Since we are not configuring CTS and RTS here, turn off

// hardware flow control. If HW flow control is used, then

// puart_flowOff should not be invoked.

puart_flowOff();

//BEGIN - puart interrupt

// The following lines enable interrupt when one (or more) bytes

// are received over the peripheral uart interface. This is optional.

// In the absense of this, the app is expected to poll the peripheral

// uart to pull out received bytes.

// clear interrupt

P_UART_INT_CLEAR(P_UART_ISR_RX_AFF_MASK);

// set watermark to 1 byte - will interrupt on every byte received.

P_UART_WATER_MARK_RX_LEVEL (1);

// enable UART interrupt in the Main Interrupt Controller and RX Almost Full in the UART

// Interrupt Controller

P_UART_INT_ENABLE |= P_UART_ISR_RX_AFF_MASK;

// Set callback function to app callback function.

puart_rxCb = application_puart_interrupt_callback;

// Enable the CPU level interrupt

puart_enableInterrupt();

/* END - puart interrupt */

}

void application_puart_interrupt_callback(void* unused)

{

   // There can be at most 16 bytes in the HW FIFO.

   char readbytes[16];

   UINT8 number_of_bytes_read = 0;

   while(puart_rxFifoNotEmpty() && puart_read(&readbytes[number_of_bytes_read]))

   {

   readBuffer[number_of_bytes_read] = readbytes[number_of_bytes_read];

   number_of_bytes_read++;

   ble_trace1("uart rx data is %d", (UINT8*)readBuffer[number_of_bytes_read]);

   }

  P_UART_INT_CLEAR(P_UART_ISR_RX_AFF_MASK);

P_UART_INT_ENABLE |= P_UART_ISR_RX_AFF_MASK;

}

0 Likes
1 Solution
Anonymous
Not applicable

I overwrite ws_upgrade_uart_init() and ws_upgrade_uart_interrupt_callback, then  the problem disappeared.

I'm not sure the root cause still.

Diff has no issue before and after.

If I can get the root cause, I'll share

View solution in original post

0 Likes
3 Replies
Anonymous
Not applicable

Have you seen this thread?

Re: puart_write() crashing on BCM20736?

Maybe it helps.

0 Likes
Anonymous
Not applicable

I should change the fist script.

it does  does NOT go entering to interrupt call back often.

0 Likes
Anonymous
Not applicable

I overwrite ws_upgrade_uart_init() and ws_upgrade_uart_interrupt_callback, then  the problem disappeared.

I'm not sure the root cause still.

Diff has no issue before and after.

If I can get the root cause, I'll share

0 Likes