- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
---------------------------------------------------------------------------------------------------
SDK: 2.2.2
Hardware: Tag3(Master) + Our Custom PCB-BCM20737S(Slave)
Firmware: hello_client + hello_sensor
---------------------------------------------------------------------------------------------------
Hi BRCM FAE,
As a continuation of this thread: Transmission times of connection event?
I'm sorry about my poor English,but I will describe my problem as much as possible.
I can got 1~4 packets in each connection event. The results are shown in fig. 1. You can see that the master send 4 packets to the slave in one connection event. The slave send 1 or 4 packets to the master . This is the result after I download the hello_client and hello_sensor to the chip.
fig.1 After download the firmware
But when I reset the master and slave, and I got different result. The results are shown in fig. 2. You can see that the master just send 1 packet in connection event, and some connection event didn't send any packet.
fig.2 After reset the MCU
The result of fig.1 and fig.2 is the same firmware. But I got different packet amount in connection event. Why has this phenomenon?
Hello_client firmware:
1. add GATT service
2. add auto scan(Because I disable GPIO interrupt)
3.change connection parameter in hello_client_create.
4.add puart function
--------------------------------------------------------------------------------------------------------------------------------------------------------------------
Hello_sensor firmware:
1. add GATT service
2. add notification callback function
3. send 15 notification packets to hello_client
4.change the Connection parameter update requeset
5. add puart function
Solved! Go to Solution.
- Labels:
-
MasterSlave
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
My colleague from Avnet (Taipei) will get in touch with you on this query.