The BCM20732 SOC Datasheet is now available here on the community...

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
3 Replies
Anonymous
Not applicable

Hi mfortner,

  Regarding to the power consumption from datasheet, is the '-9.1' a type error?

  Also, in which condition that the max consumption for RX part behaved?

0 Likes

Typo.

10mA peak is the current at the battery terminals when a DC-DC is used to supply 1.2V to the core and RFsupplies during an active TX/RX. When the Cortex M3 is running (no RF activity), the current draw should be under ~2mA or lower at the battery terminals.

Anonymous
Not applicable

I suggest to cut the wires to the buzzer if you are using the TAG board and want to measure current consumption.