- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I hope to get answers to the following two questions.
I enabled external 32KHz LPO on TAG03 board by connecting it to BCM20737.
I have the following function call in my app but the app seems to work fine with or without it. Is the call absolutely necessary?
bleapputils_changeLPOSource(LPO_32KHZ_OSC, FALSE, 250);
Also, my app has a part where enters deep sleep.
The part has the following statement before calling devlpm_enterLowPowerMode(). Is this assignment absolutely necessary?
devLpmConfig.wakeFromHidoffRefClk = HID_OFF_TIMED_WAKE_CLK_SRC_32KHZ;
- Labels:
-
Clocks (InternalExternal)
-
Sleep Modes
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
Hello j.t,
Thank you for the post.
However, I don't use RTC.
Do I still have to explicitly select ext 32KHz LPO in the source code?
BR,
Wataru Sugimoto
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Helloi Wataru,
Please loot at the rtc_sample code in the SDK:
// If we need to use the external 32K, then configure the reference
rtcConfig.oscillatorFrequencykHz = RTC_REF_CLOCK_SRC_32KHZ;
// Since the 32K external LPO is connected tp P10, P11, P12, P26 and P27,
// input and putput disable all 5 GPIOs.
gpio_configurePin(0, 10, GPIO_INPUT_DISABLE, 0);
gpio_configurePin(0, 11, GPIO_INPUT_DISABLE, 0);
gpio_configurePin(0, 12, GPIO_INPUT_DISABLE, 0);
gpio_configurePin(1, 10, GPIO_INPUT_DISABLE, 0);
gpio_configurePin(1, 11, GPIO_INPUT_DISABLE, 0);
// Initialize the RTC.
Thanks
JT