My understanding is the connection timeout error is supposed to happen
after supervision timeout which is 500 ms in my application.
The problem is scan no longer works once the connection timeout (0x8) occurs.
My application is the Initiator of the connection and
emconinfo_getDiscReason() returns 0x8 on connection down callback.
Can you provide some advice to debug this issue?
I am using 20737 with SDK 2.1.1
Here are my scan parameters.
blecen_cen_cfg.scan_type = HCIULP_PASSIVE_SCAN; |
blecen_cen_cfg.scan_adr_type = HCIULP_PUBLIC_ADDRESS;
blecen_cen_cfg.scan_filter_policy = HCIULP_SCAN_FILTER_POLICY_WHITE_LIST_NOT_USED;
blecen_cen_cfg.filter_duplicates = HCIULP_SCAN_DUPLICATE_FILTER_OFF;
blecen_cen_cfg.init_filter_policy = HCIULP_INITIATOR_FILTER_POLICY_WHITE_LIST_NOT_USED;
blecen_cen_cfg.init_addr_type = HCIULP_PUBLIC_ADDRESS;
blecen_cen_cfg.high_scan_interval = 1500; //slots |
blecen_cen_cfg.low_scan_interval = 1500; //slots
blecen_cen_cfg.high_scan_window = 100; //slots
blecen_cen_cfg.low_scan_window = 100; //slots
blecen_cen_cfg.high_scan_duration = 300; //seconds
blecen_cen_cfg.low_scan_duration = 300; //seconds
blecen_cen_cfg.high_conn_min_interval = 8; //frames |
blecen_cen_cfg.low_conn_min_interval = 8; //frames
blecen_cen_cfg.high_conn_max_interval = 8; //frames
blecen_cen_cfg.low_conn_max_interval = 8; //frames
blecen_cen_cfg.high_conn_latency = 0; |
blecen_cen_cfg.low_conn_latency = 0;
blecen_cen_cfg.high_supervision_timeout = 50;
blecen_cen_cfg.low_supervision_timeout = 50;
blecen_cen_cfg.conn_min_event_len = 0;
blecen_cen_cfg.conn_max_event_len = 0;
Solved! Go to Solution.
Hi Hardy,
Thanks for your help. I think it is really worth trying your suggestion.
By the way, the connection timeout (0x8) is no longer observed after switching to our newly designed board.
Therefore, this issue is not reproducible any longer.
Perhaps it was triggered by some board related issues or instability of hardware?
Found the following codes from a4wp_power_transmitter sample app.
if (emconinfo_getDiscReason() == BLEPTUM_HCI_ERR_CONNECTION_TIMEOUT) | |
{ |
#ifdef BLEPTUM_HCI_RESET
if(bleprofile_p_cfg->disc_required & BLEPTUM_HCI_RESET) | |
{ | |
blecm_hciReset(); | |
ble_trace0("HCI_Reset"); | |
} |
#endif
#ifdef BLEPTUM_WDTO
if (bleprofile_p_cfg->disc_required & BLEPTUM_WDTO) | |
{ | |
ble_trace0("Watchdog_timeout"); | |
// infinite loop to trigger WD reset | |
while(1); | |
} |
#endif
} |
Is it recommended to do HCI reset or Watchdog reset on Connection Timeout?
Are you powering off the slave right after the connection to get to the timeout?
I would try to call: blecm_disconnect(BT_ERROR_CODE_CONNECTION_TERMINATED_BY_LOCAL_HOST); when you receive the link down callback. I may help to clear a state in the stack.
Hi 79rpm,
Thanks for your advice.
I am getting the connection timeout in Master while receiving Notification data from Slave.
According to BLE sniffer trace, Master suddenly stops sending POLL frame (header only) to Slave.
Notification data interval is 10 ms in my use case.
Just tried blecm_disconnect() as you suggested, the scan issue still occurs.
A similar symptom of the fatal error has been observed after LMP RESPONSE TIMEOUT (0X22).
Is there any to work around this issue? Or anyway to reduce the chance of this error?
Hi mkim,
Not sure about the reason of your case, but would you try to have kind of reset state machine as posted here Problem when client disconnection during Indication/confirmation phase. ?
Hi Hardy,
Thanks for your help. I think it is really worth trying your suggestion.
By the way, the connection timeout (0x8) is no longer observed after switching to our newly designed board.
Therefore, this issue is not reproducible any longer.
Perhaps it was triggered by some board related issues or instability of hardware?