Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Anonymous
Not applicable

I have tried the examples provided for the SDK 2.0.1 on the BCM92073X_LE_KIT.

I have yet to see anything output to my tera term, and I don't get any echo back with I enter a key.

Is there an specific example that should work?

Do I need to set up anything in specific, other than building/downloading the image.

-Thanks, Mike

1 Solution

<<<Is there any way to capture the Broadcom Debug Viewer console data to file?

I could not find a way to configure Eclipse to log the console data to file.  However, you can right-click in the window, clear the trace buffer, ... let the debug information flow, and flow, and flow.... then use the lovely CTRL-A (select all), CTRL-C to copy, and then Cut-Paste it elsewhere (CTRL-V)!     Sorry!

Note: I've attached what the console-debug data looks like when the Eclipse Debug Plugin (from Broadcom) is running, versus what you'd see if you used a terminal program to capture the debug messages.  It shows you pretty much want to use the plugin...

Without the plugin (captured w/TeraTerm):

tones_create()

Buzzer init count: 0x200, Toggle Count: 0x2FF

LED init count: 0x19A, Toggle Count: 0x308

@$*#04FFF6F70092011E0300C1E804100000008003BE1A000000008003AE1A1

60000008003B21A020000008003B61A100010008003BA1A002A00008003BE1A

000000008003AE1A170000008003B21A020000008003B61A050005008003BA1

A032800008003BE1A000000008003AE1A180000008003B21A020000008003B6

.

.

.

F1EF700920103000007362A0100E80300073A2A500000000007522A50000100

With the plugin doing the decryption::

10:05:10 - tones_create()

10:05:10 -

10:05:10 - 0118

10:05:10 - 0018

10:05:10 - 021600002a

10:05:10 - 50574d20546f6e657300000000000000

10:05:10 - 021800012a

10:05:10 - 0002

10:05:10 - 0201060a0950574d20546f6e6573

10:05:10 - 020a04

10:05:10 - Buzzer init count: 0x200, Toggle Count: 0x2FF

10:05:10 -

10:05:10 - LED init count: 0x1EE, Toggle Count: 0x3B4

10:05:10 -

10:05:10 -

10:05:10 - blecm evt handler:

10:05:10 - 0e0401082000

10:05:10 -

10:05:10 - blecm evt handler:

10:05:11 - 0e0401092000

10:05:11   Trace Decoding Error - Could not find line number 314

10:05:11   Attribute bytes

10:05:11   Handle: 0016

10:05:11   Perm  : 0002

10:05:11   Len, Max Len : 0010, 0010

10:05:11   UUID  : 2A00

10:05:11   Attribute bytes

10:05:11   Handle: 0017

10:05:11   Perm  : 0002

10:05:11   Len, Max Len : 0005, 0005

10:05:11   UUID  : 2803

10:05:11   Attribute bytes

10:05:11   Handle: 0018

10:05:11   Perm  : 0002

10:05:11   Len, Max Len : 0002, 0002

10:05:11   UUID  : 2A01

10:05:11   Attribute bytes

10:05:11   Gatt DB Dump complete

10:05:11   bd_addr[5:2] = 20 73 7A 1C

10:05:11   bd_addr[1:0] = 9308 00

10:05:11   GPIO 0001 (11)

10:05:11   GPIO 0000 (104)

10:05:11   GPIO 0014 (1003)

10:05:11   GPIO 0015 (20)

10:05:11   Interrupt mask[0,1]:0001 0000

10:05:11   Interrupt mask[2]:0000

10:05:11   GPIO_WP:OFF= 00

10:05:11   GPIOBTN1:OFF=1,INT:0

10:05:11   GPIO_LED:OFF=1

10:05:11   GPIOBAT

10:05:11   Fine Timer(1000 ms, 1/sec)

10:05:11   Fine TImer tick 80

10:05:11   Normal Timer(0 s, 0 tick)

View solution in original post

12 Replies
ArvindS_76
Employee
Employee
500 likes received 250 likes received 100 likes received

Did you try the uart_firmware_upgrade application? You should be able to modify it to output ASCII text instead of implementing the download/upgrade mechanism if you just want to test reading from/writing to the uart.

0 Likes
ShawnA_01
Employee
Employee
25 solutions authored 10 solutions authored 5 solutions authored

You may not have seen any output in TeraTerm due to the new debug/printf mechanism in SDK2 as shown below.

If you do not have the "Trace" pull-down available, you are still running the SDK1.

6-5-2014 10-37-23 AM.png

Anonymous
Not applicable

Is there any way to capture the Broadcom Debug Viewer console data to file? It seems the capture option goes away once the trace is started.

toolbar.png

Another option would be to be able to disable the lower level TRACE messages at compile time so a regular terminal could be used. Is something like that possible?

0 Likes

<<<Is there any way to capture the Broadcom Debug Viewer console data to file?

I could not find a way to configure Eclipse to log the console data to file.  However, you can right-click in the window, clear the trace buffer, ... let the debug information flow, and flow, and flow.... then use the lovely CTRL-A (select all), CTRL-C to copy, and then Cut-Paste it elsewhere (CTRL-V)!     Sorry!

Note: I've attached what the console-debug data looks like when the Eclipse Debug Plugin (from Broadcom) is running, versus what you'd see if you used a terminal program to capture the debug messages.  It shows you pretty much want to use the plugin...

Without the plugin (captured w/TeraTerm):

tones_create()

Buzzer init count: 0x200, Toggle Count: 0x2FF

LED init count: 0x19A, Toggle Count: 0x308

@$*#04FFF6F70092011E0300C1E804100000008003BE1A000000008003AE1A1

60000008003B21A020000008003B61A100010008003BA1A002A00008003BE1A

000000008003AE1A170000008003B21A020000008003B61A050005008003BA1

A032800008003BE1A000000008003AE1A180000008003B21A020000008003B6

.

.

.

F1EF700920103000007362A0100E80300073A2A500000000007522A50000100

With the plugin doing the decryption::

10:05:10 - tones_create()

10:05:10 -

10:05:10 - 0118

10:05:10 - 0018

10:05:10 - 021600002a

10:05:10 - 50574d20546f6e657300000000000000

10:05:10 - 021800012a

10:05:10 - 0002

10:05:10 - 0201060a0950574d20546f6e6573

10:05:10 - 020a04

10:05:10 - Buzzer init count: 0x200, Toggle Count: 0x2FF

10:05:10 -

10:05:10 - LED init count: 0x1EE, Toggle Count: 0x3B4

10:05:10 -

10:05:10 -

10:05:10 - blecm evt handler:

10:05:10 - 0e0401082000

10:05:10 -

10:05:10 - blecm evt handler:

10:05:11 - 0e0401092000

10:05:11   Trace Decoding Error - Could not find line number 314

10:05:11   Attribute bytes

10:05:11   Handle: 0016

10:05:11   Perm  : 0002

10:05:11   Len, Max Len : 0010, 0010

10:05:11   UUID  : 2A00

10:05:11   Attribute bytes

10:05:11   Handle: 0017

10:05:11   Perm  : 0002

10:05:11   Len, Max Len : 0005, 0005

10:05:11   UUID  : 2803

10:05:11   Attribute bytes

10:05:11   Handle: 0018

10:05:11   Perm  : 0002

10:05:11   Len, Max Len : 0002, 0002

10:05:11   UUID  : 2A01

10:05:11   Attribute bytes

10:05:11   Gatt DB Dump complete

10:05:11   bd_addr[5:2] = 20 73 7A 1C

10:05:11   bd_addr[1:0] = 9308 00

10:05:11   GPIO 0001 (11)

10:05:11   GPIO 0000 (104)

10:05:11   GPIO 0014 (1003)

10:05:11   GPIO 0015 (20)

10:05:11   Interrupt mask[0,1]:0001 0000

10:05:11   Interrupt mask[2]:0000

10:05:11   GPIO_WP:OFF= 00

10:05:11   GPIOBTN1:OFF=1,INT:0

10:05:11   GPIO_LED:OFF=1

10:05:11   GPIOBAT

10:05:11   Fine Timer(1000 ms, 1/sec)

10:05:11   Fine TImer tick 80

10:05:11   Normal Timer(0 s, 0 tick)

Anonymous
Not applicable

Thanks for your quick response Shawn.

Do you know if it is possible to run the plugin from the command line? That way, the output could be redirected to someplace useful.

What do the Broadcom developers do?

0 Likes

We are checking on the feasibility of improving the plugin to enable logging. 

0 Likes

Hello kwilloughby

I received and tested a new Eclipse plugin that has the ability to log to file.  It's a no-frills implementation, but it does work.  Let me see how the team wants to release it... in the interim, I have a question for you.

You had provided a screen-shot (red / green arrows) that had some additional icons on your console pane.  My fresh installation of the SDK does not have these!  I could not figure out how to enable them.

How did you get them?

icons.png

0 Likes
Anonymous
Not applicable

Hi Shawn,

I did nothing special to enable those controls. Those show up in the CDT build console, which shows the output from the build process. I think that they enable you to step through build errors? The don't show up when debug traces are running.

Ken

0 Likes

SDK 2.0.1 and earlier does not have the (debug/console window) logging feature.  It is targeted for the next SDK release.  If you must have it before then, send me a private message with your email address.

0 Likes
Anonymous
Not applicable

I'm good for right now. I look forward to seeing it in the next SDK release.

0 Likes
Anonymous
Not applicable

I don't see the "Trace" menu on OS X. Is that only for Windows?

0 Likes

Are you running SDK 2.0.1?   (you can open the ~WICED-Smart-SDK/version.txt file to find out)

0 Likes