Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hello, guys.

1. I use two BLE starter kit BCM20737TAG. One in host mode and other in slave mode. After connecting slave TAG to the host TAG and save to NV memory address of the connected host and sending data I turn into a deep sleep. After pressing on the user button SW1 (waking up due interrupt GPIO) restarts slave TAG. Please, tell me, how to determine what slave TAG start came from the deep sleep mode to exclude paring (send advertising) again? May be there is an example implementation?

2. As I read on the community going to deep sleep mode is only possible in not connected state. How to perform explicitly disconnect slave from the host?

3. What API functions are used to going to simple sleep and waking up from in?

Thanks in advance for your replies

1 Solution
Anonymous
Not applicable

1. The connection is started only by the central.

And advertising triggers central to make the connection.

The application can't know whether waken up from deep sleep mode.

So I think reading host address from NVRAM helps this.

2. To disconnect peripheral from central, please refer below thread.

disconnect recipe (from central) when multiple peripherals are connected

3. Entering sleep mode is managed by firmware.

The application can disable entering sleep mode using devlpm_registerForLowPowerQueries()

View solution in original post

9 Replies
Anonymous
Not applicable

1. The connection is started only by the central.

And advertising triggers central to make the connection.

The application can't know whether waken up from deep sleep mode.

So I think reading host address from NVRAM helps this.

2. To disconnect peripheral from central, please refer below thread.

disconnect recipe (from central) when multiple peripherals are connected

3. Entering sleep mode is managed by firmware.

The application can disable entering sleep mode using devlpm_registerForLowPowerQueries()

MichaelF_56
Moderator
Moderator
Moderator
250 sign-ins 25 comments on blog 10 comments on blog

For item 3, this thread contains examples of how to go into sleep and come out: Putting '20732S into sleep or deep sleep mode

JT's blog is also an excellent source of information for Sleep and Deep Sleep Techniques: Sleep Deep_Sleep Explanation and Techniques

Anonymous
Not applicable

Hi, all

I changed example hello_sensor so that every 10 seconds after the connection to the host and sending data occurs to go to deep sleep by follows:

// Give app chance to reprogram GPIO Interrupt sources or whatever

// it needs to do before going HID Off

bleprofile_enteringDiscLowPowerMode(DEV_LPM_DISC_LOW_POWER_MODES_HID_OFF);

// We can go hid-off

mia_enterHidOff(0, devLpmConfig.wakeFromHidoffRefClk);

// If we get here HID-OFF was aborted

bleprofile_abortingDiscLowPowerMode(DEV_LPM_DISC_LOW_POWER_MODES_HID_OFF);

To wake up from deep sleep, I use the user button SW1 (GPIO Interrupt). It is reset TAG3.

The problem is that during the second and subsequent attempts to go to sleep mode that not occurs.

In traces displays the following:

enterHidoff!!!

Prepare Power save

noAdv

Start Power Save

TimersKilled

abortHidoff!!!

Stop Power Save

Fine Timer(1000 ms, 1/sec)

Fine TImer tick 80

Normal Timer(0 s, 0 tick)

SMP Conn Down

connDown

ConnDnStopIdlTmr

What is the reason?

P.s.

Below I show the pictures of current consumption in my example

!dsleep_questions.jpg

Wonder why this is ADV and connection time rather big (~ 0.8 - 3 sec).

Did I understand correctly that the standby - this automatic sleep mode?

I suspect your request to enter HIDOFF is not being honored.

Check out:  How to enter HIDOFF? How to detect if the request is not honored? and also Re: System sometimes draws 3mA after entering HIDOFF mode

You may also want to make sure you are not getting bitten by the crystal warmup issue:  Re: BCM20732S module keeps crashing

Have you had a chance to investigate the two options recommended on the 25th of July by santol?

  • Verification that HIDOFF is being honored
  • Crystal Warmup as a potential problem

Let us know if you have made any progress on this issue?

alexander.pisarevskiy j.t arvinds pnorbury

Here is some source code I received from the development team which demonstrates deep sleep enablement and the associated clock source handling: Source Code: deep sleep enablement and the associated clock source handling....

Maybe this will help.

This will also eventually be added to the Sleep Blog mentioned earlier.

Anonymous
Not applicable

Hi Guys,

  I would like to understand if there was a resolution to Andrei's question?  I have run into the same scenario myself in which after the first time of going into DEEP_SLEEP the device continually wakes up repeatedly and provides the same Debug Message output.  I have reviewed the source code in the example and incorporated everything that would need to be in the app and after the initial DEEP_SLEEP it continually wakes up unexpectedly.  I am not using a Timed wakeup just a GPIO Pin interrupt.  I have tried this on the TAG3 board and the Embedded Masters EMRF-20736 board and both produce the same results?  A bit baffled...

Regards,

Frank

Anonymous
Not applicable

Resolved it by pulling P0 HIGH...

Thanks for confirming.

santol had a couple of posts regarding this that have helped a few others with the same problem.

Here's one of them: How to enter HIDOFF? How to detect if the request is not honored?