Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Anonymous
Not applicable

Hello,

I have a problem programming my BCM920737TAG.

When i programming my board this is the result:

pastedImage_2.png

I have used a different USB lead to rule this out.

Also i am able to receive the debug data back when i go into debug mode and switch number 2 off on sw4.

When programming, all the switches are in the on position in sw4. I press the restart button on the board before trying to program and make sure i am not in debug mode.

I have uninstalled the WICED SDK and re downloaded it and installed it but was no luck.

I also have a second board which i tried it on and have the same problem. I do not believe it to be a hardware issue or programming sequence.

I believe it could be something to do with a driver or the wiced IDE.

I have also had a good at doing a reboot but this does not work either.

Any information would be great.

Regards,

Luke.

2 Replies
MichaelF_56
Moderator
Moderator
Moderator
250 sign-ins 25 comments on blog 10 comments on blog

-Do you see two COM ports enumerating within Windows device manager when you plug the TAG3 board into the USB port?

-Have you tried the recovery process outlined in the WICED Smart Quick Start Guide (SDK 2.x and TAG3 Board)​?

-Is this a custom application or one of the defaults that install with the SDK?

The good news is that the TAG3 board is fairly robust, so the goal here is to get it back to it's factory state then slowly add custom pieces to determine what is causing this issue.

jakewtorres

0 Likes
BoonT_56
Employee
Employee
500 likes received 250 likes received 100 likes received

Is this still an issue?

llynch

0 Likes