Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hi,

There are two TX tests available in MBT:

- LE Transmitter Test

- Continuous Transmit Test

The Continuous Transmit test allows you to set a power output level in dBm but the LE Transmitter Test doesn't.

What is the default power output set to with the LE Transmitter test?

0 Likes
1 Solution
ShawnA_01
Employee
Employee
10 questions asked 5 comments on KBA First comment on KBA

The "LE Transmitter test" is a standard test that requires the testing be done at the maximum power level the device is capable of doing.  This is why MBT does not allow the command line parameter to change it.  (The full source to MBT is found in the SDK).


As shown in the datasheet, the output will not exceed +4dBm.

View solution in original post

0 Likes
2 Replies
ShawnA_01
Employee
Employee
10 questions asked 5 comments on KBA First comment on KBA

The "LE Transmitter test" is a standard test that requires the testing be done at the maximum power level the device is capable of doing.  This is why MBT does not allow the command line parameter to change it.  (The full source to MBT is found in the SDK).


As shown in the datasheet, the output will not exceed +4dBm.

0 Likes
Anonymous
Not applicable

Great, thanks.

0 Likes