Hello,
I saw in a couple threads mentioning that the power consumption when a peripheral is connected, but not doing anything should be in the uA range. However my device seems to be running in the 10mA range always.
How can I enable low power modes? I was able to but the device into deep sleep, but at that point the connection is lost.
Do you have a recommended way to measure power consumption on the TAG board?
Solved! Go to Solution.
Hello ppaszkow,
Measurements on the TAG Boards:
BCM20736 TAG003 Board:
To measure I/O Current:
BCM20732 TAG002 Board:
Let us know if this answers your questions.
JT
Could you explain the use case in question. Depending on your advertisement interval, our device can use different sleep modes:
According to the team, 11mA (11uA would seem more inline) for connected non-advertising mode seems high.
What else is connected and how exactly are you measuring current?
The SW configuration is pretty much same as the hello sensor example.
Since my post I did realize that the 11mA is not accurate, (there are other devices that are drawing some current, this is on our custom board). But still it seems that the module is using about 5mA.
In my case I am powering the board with a DC power analyzer that displays the current consumption.
I am not seeing anything in the uA range unless I go to deep sleep.
Could you suggest how to measure current on the TAG board? That way we can be sure we are comparing the same thing.
We have a team working on this internally, so one of them should be able to respond shortly.
Thanks in advance for your patience.
Hello ppaszkow,
Measurements on the TAG Boards:
BCM20736 TAG003 Board:
To measure I/O Current:
BCM20732 TAG002 Board:
Let us know if this answers your questions.
JT
Thank you. I will give this a try and get back to you.
I have read BCM20732S datasheet, its table-5 told me that transmission current is 9.3mA, why is "during RF activity ~22mA."?
Not sure of the context under which that value is provided.
For now, the following table 5 values within the datasheet should be used when making power calculations.
We are also working on publishing more detailed power values (with use cases)