I tried to modify hello_client and hello_sensor (BCM20737 TAG) to build a piconet:
Master <-> Relay <-> Slave
I use hello_client codes for Master and Relay. hello_sensor codes for Slave.
I can make it work when there is no bonding/encryption enabled. However, when I enable the encryption, there is a problem between Master and Relay.
The sniffer shows the following:
Master -> Relay: Pairing Request
Relay -> Master: Pairing Response
Master -> Relay: Pairing Confirmation
Relay -> Master: Pairing Random
then there is no further control messages for encryption. The link is still there (timeout disabled) but no more control messages.
I can make the Master (hello_client) connects with Slaves (hello_sensor) with encryption. However, I cannot make the Master (hello_client) connects with Relay (hello_client) with encryption.
Any idea why is that? Any difference of the security operations between hello_client (as slave) and hello_sensor?
Solved! Go to Solution.
I still cannot figure out why I cannot use the codes from "hello_client" as a relay with encryption connection. When the encryption is disabled, it can function as a relay. I later modified the codes of "hello_sensor" to make it as a relay (master/slave) node and it has no problem.
Below is a good thread on simultaneous roles of the BLE, that your Relay is performing.
So is this still an issue?
I still cannot figure out why I cannot use the codes from "hello_client" as a relay with encryption connection. When the encryption is disabled, it can function as a relay. I later modified the codes of "hello_sensor" to make it as a relay (master/slave) node and it has no problem.