Hello,
I am upgrading the installation from WICED Smart SDK2.2.2 to 2.2.3. Compiling a sample code gives me the following:
dyld: Library not loaded: /System/Library/Perl/5.12/darwin-thread-multi-2level/CORE/libperl.dylib
I do not have /System/Library/Perl/5.12 installed. libperl.dylib is available under 5.18 (as well as 5.16):
/System/Library/Perl/5.18/darwin-thread-multi-2level/CORE/libperl.dylib
I do not have an option to easily change the content of /System/Library/Perl on MacOSX.
Please provide a solution (or possible configuration) to get the this problem solved.
BTW there is a similar post on this here (I installed WICED Smart IDE 2.1.1 on OSX Yosemite - Problems ).
Solved! Go to Solution.
Did you try this?
cd /System/Library/Perl
sudo ln -s 5.18 5.12