Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Smart Bluetooth Forum Discussions

Anonymous
Not applicable

How do i configure peripheral UART

I want to use P_UART for communicating with other MCU & DEBUG_UART for DEBUGGING.

Thanks ,

Shrikrishna.

0 Likes
4 Replies
MichaelF_56
Moderator
Moderator
Moderator
250 sign-ins 25 comments on blog 10 comments on blog

Take a look at the following sample application: /WICED-Smart-SDK/Apps/puart_control

I believe this provides an example of what you are trying to accomplish.

There is @puart_control AppNote in the SDK as well under /WICED-Smart-SDK/Apps/puart_control/PUART-Control.pdf

0 Likes
JacobT_81
Employee
Employee
250 likes received 100 likes received 50 likes received

If you're attempting to set these up simultaneously you'll run into problems. UART protocol doesn't support multi-slave implementations.

1. For PUART traces, insert in your APLLICATION_INIT() after bleapp_set_cfg:

          BLE_APP_ENABLE_TRACING_ON_PUART();

Ensure that your pin numbers are properly configured in the puart_cfg table:

          // Following structure defines UART configuration

          const BLE_PROFILE_PUART_CFG wiced_sense_puart_cfg =

          {

              /*.baudrate   =*/ 115200,

              /*.txpin      =*/ GPIO_PIN_UART_TX,

              /*.rxpin      =*/ GPIO_PIN_UART_RX,

          };

2 .PUART Communication with other MCU:

     As mwf_mmfae​, said the puart_control app in the SDK demonstrate an extremely detailed interface.

    

     For a more basic understanding of PUART implementation see: Connecting an external board to the BCM2073X via the PUART.

Jacob

Anonymous
Not applicable

Is it Possible to use Both UART simultaneously(One for DEBUG & Other for communication with other MCU)?

0 Likes

The HCI UART for all intents and purposes is a programming interface only.  You can also route debug traces to the HCI UART per the instructions in the WICED Smart Quick Start Guide (SDK 2.x and TAG4 Board), but again, if you application requires some form of UART access, only the peripheral UART is available to the application.