- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I'm implementing OTAFU with BCM920737 TAG connecting USB.
I read WICED Secure Over-the-Air Firmware Upgrade Application Note (SDK 2.1 and TAG3 Board) and I'm using Android Sample provided in :WICED Smart BCM92073X OTA Firmware Upgrade (1) and WICED Smart BCM92073X OTA Firmware Upgrade (2).
When ota_firmware_upgrade sample runs, the OTAFU is success. However, in my BCM20737S application, the OTAFU fails at the last moment. The sending data percentage becomes 100% but a pop-up showing OTAFU fails appears. To make matters worse, I have to recovery. So, I think there are some problems in my application but I can't find the cause.
I attach two files indicated in console in Android Studio.
A red sentence is different from two applications.(Some green text are my own device address.)
Please help me. I couldn't identify the cause of this problem.
Best Regards
Solved! Go to Solution.
- Labels:
-
Over The Air Upgrades - OTA
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
Adding maxsong, the gentleman that provided the sample code that you are struggling with.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi gell
As the log shown (mark as RED), writing characteristic is failed, the error code is 13 it means that attribute value length is invalid.
Could you help to provide the WICED Smart device side's source codes and log?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Y I,
1. The problem we see with the OTAFU is when the new App is larger than will fit into the EEPROM.
2. What is the size of the image?
3. Are you downloading the .ota.bin file?
Thanks
JT
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
Great news. Thanks for updating the discussion!