- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I'm using a BCM20737TAG and Plugable USB Bluetooth 4.0 Low Energy Micro Adapter to test OTA feature. It used to work.
Today I found OTA failed because CRC verification failed in ws_upgrade_verify().
I print the data written to EEPROM and read from EEPROM. They're different.
bleappfwu_readMem and bleappfwu_writeMem always return 0.
This is the DS location.
Active DS1: 0x00000580, Upgrade DS2: 0x00008000.
I tried recover, it succeed. But OTA still failed.
When DIP switch 2 of SW4 is in OFF position, reset BT, it can boot.
When DIP switch 2 of SW4 is in ON position, reset NT, it won't boot. But I can still download application to the board. This is very weird.
I feel BT cannot write to EEPROM after 0x00008000.
Is there a way to download application to DS2 using UART?
Thanks you
Jeffrey
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Finally I got it working, I need turn DIP switch 1-4 of SW4 to OFF position.
The problem is I cannot see the debug trace from BT firmware