Murata-Type 1GR(CYW20736) + STM32F412 WICED development setup

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hi we are planning to use BLE module from Murata(Type 1GR) with CYW20736 and interface it externally with STM32F412 to write our application , Can you let me know which platform on WICED I need to use for the development. If their are any EVK available for this?

0 Likes
1 Solution
MichaelF_56
Moderator
Moderator
Moderator
250 sign-ins 25 comments on blog 10 comments on blog

Unfortunately there is not. An external processor could interface to the part using the peripheral UART interface.

View solution in original post

3 Replies
MichaelF_56
Moderator
Moderator
Moderator
250 sign-ins 25 comments on blog 10 comments on blog

Unfortunately there is not. An external processor could interface to the part using the peripheral UART interface.

Anonymous
Not applicable

So this module can only be used with AT commands via UART ??

0 Likes

The part is primarily designed to run self contained in embedded mode as the stack, drivers, patches, etc. are integrated into ROM.  I believe there is also close to 30K in RAM for the application to run on the internal CM3. The AT command set is not supported by default.

More here: WICED Smart Hardware Interfaces