- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Continuation of this thread: More appFineTimer questions...
I saw 12.5 ms in the comment above bleprofile_regTimerCb() function and it confused me.
If I set fine_timer_interval as 12, what will be the actual interval? 12 or 12.5 ms?
If I really want the interval to be 12.5 to make it perfectly fit in every 1 second, how can I config it?
Solved! Go to Solution.
- Labels:
-
Timers
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi JT,
Because fine_timer_interval is UINT16, 12.5 will not fit in the variable.
I've tested the length of one fine interval using bleapputils_currentNativeBtClk and bleapputils_BtClksSince.
I have found that the interval will always be floored to multiple of 12.5 ms.
For example,
If the value of fine_timer_interval is in the range of 1 - 24, the actual interval will be 12.5 ms.
For the range of 25 - 37, the actual interval will be 25 ms.
For the range of 38 - 49, the actual interval will be 37.5 ms.
This is a bit tricky. If you put 37.5 in the fine_timer_interval. The actual interval you get will be 25 ms.
Thanks,
Koon