I have 2 questions regarding the Le Receiver Test using MBT.
Once the command is sent to the UART is it allowed to disconnect the FTDI module from the device.
The reason I am asking is because I assume since a laptop is used to send the command it would make sense
to leave the device alone in a test chamber without the host attached to it.
Or does the host must be connected at all time because some data will be sent periodically to the UART and
such data must be recorded to acknowledge that the test passed.
Finally would you know the maximum USB to UART cable length for an FTDI module to be used with MBT test
without losing data during the test ?
Have anyone tried those cable to run MBT ?
Solved! Go to Solution.
Thanks during testing to 15.109 using
LE Receiver Test batch file
The lab finished the testing to 15.109 this morning and when testing in the 1-4 GHz range, they noticed that there were transient bursts in the 2.4 ISM band
It appears the .bat file I provided does not actually place the radio into receive mode but LE Receiver Test. I assume this because the spectrum appears to show that the transmissions are “advertising channel” bursts.
Looking at the screen shot it reflected that the device was in normal operation mode following the execution of the FW
Please note that the FW was flashed in the board used for test but I assumed that using MBT tool
will bypass the running mode of the FW
Reading the PDF documenation it says
Configure the CYW2070X to run in the HCI mode.
a. When a CYW2070X device starts up it searches for an HCI UART.
b. If detected, the device stays in the HCI mode.
It can be tricky to make sure the device is in HCI mode.
Since the device can be powered by 2AA battery but we didn't put a PGM/RUN switch on the designed to force it to stay in HCI/PGM mode here is the sequence used during FCC
Note regarding mbt receive_only command
Receive Only : this command is no longer available in latest version of mbt.exe so the documentation is off....
Instead use the LE test using channel # this command is working
This test issues a command to the CYW2070X to set the radio to camp on a specified frequency. The frequency
on which the device listens for packets is passed as a parameter.
The command usage used to be:
mbt receive_only <rx_frequency>
where:
rx_frequency: 2402 MHz to 2480 MHz
The example below instructs the CYW2070X to set the receiver to a frequency of 2406 MHz.
Would the following command properly place the device in receive only.
Is it neede to send a reset command first ?
WICED-Smart-SDK\Tools\mbt\win32>mbt COM3 receive_only 2406
Sending HCI Command:
0000 < 01 2B FC 01 06 >
Received HCI Event:
0000 < 04 0E 04 01 2B FC 00 >
Success
This would be nice for Cypress to offer a bunch of FW app for each FCC test case to put the device in test mode at boot time instead of relying on mbt
and the ROM
You may remove the ftdi module once you execute and download the test command. The device will be in test mode and work as your test command has intended. Then do you intend to connect the ftdi module back to terminate the test? Or simple just interrupt the power supply?
82ft is way too long and you will likely encounter reliability issue. Do refer to section 4 of the below link in which we described how
we use a programming cable (from FTDI) to do this.
Thanks during testing to 15.109 using
LE Receiver Test batch file
The lab finished the testing to 15.109 this morning and when testing in the 1-4 GHz range, they noticed that there were transient bursts in the 2.4 ISM band
It appears the .bat file I provided does not actually place the radio into receive mode but LE Receiver Test. I assume this because the spectrum appears to show that the transmissions are “advertising channel” bursts.
Looking at the screen shot it reflected that the device was in normal operation mode following the execution of the FW
Please note that the FW was flashed in the board used for test but I assumed that using MBT tool
will bypass the running mode of the FW
Reading the PDF documenation it says
Configure the CYW2070X to run in the HCI mode.
a. When a CYW2070X device starts up it searches for an HCI UART.
b. If detected, the device stays in the HCI mode.
It can be tricky to make sure the device is in HCI mode.
Since the device can be powered by 2AA battery but we didn't put a PGM/RUN switch on the designed to force it to stay in HCI/PGM mode here is the sequence used during FCC
Note regarding mbt receive_only command
Receive Only : this command is no longer available in latest version of mbt.exe so the documentation is off....
Instead use the LE test using channel # this command is working
This test issues a command to the CYW2070X to set the radio to camp on a specified frequency. The frequency
on which the device listens for packets is passed as a parameter.
The command usage used to be:
mbt receive_only <rx_frequency>
where:
rx_frequency: 2402 MHz to 2480 MHz
The example below instructs the CYW2070X to set the receiver to a frequency of 2406 MHz.
Would the following command properly place the device in receive only.
Is it neede to send a reset command first ?
WICED-Smart-SDK\Tools\mbt\win32>mbt COM3 receive_only 2406
Sending HCI Command:
0000 < 01 2B FC 01 06 >
Received HCI Event:
0000 < 04 0E 04 01 2B FC 00 >
Success
This would be nice for Cypress to offer a bunch of FW app for each FCC test case to put the device in test mode at boot time instead of relying on mbt
and the ROM
I actually tested the 65 ft USB cable connected to a regular FTDI cable and it seams to work fine.
I was able to put the device in receive only mode
C:\Users\thomas\Desktop\FCC>le_receiver_test_ch39.bat
"mbt le_receiver_test COMx <rx_channel>"
" rx_channel = (F - 2402) / 2"
" Range: 0 - 39. Frequency Range : 2402 MHz to 2480 MHz"
Sending HCI Command:
0000 < 01 03 0C 00 >
Received HCI Event:
0000 < 04 0E 04 01 03 0C 00 >
Success
Sending HCI Command:
0000 < 01 1D 20 01 27 >
Received HCI Event:
0000 < 04 0E 04 01 1D 20 00 >
Success
LE Receiver Test running, to stop execute le_test_end