Is there a date to Update the 2.2.1 installer to fix the JRE version code bug, so it will install on Windows 10?

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Is there a date to Update the 2.2.1 installer to fix the JRE version code bug, so it will install on Windows 10?

This has been an open issue for quite a while.

I documented this as an installer bug some time ago. See my other post.

Joe

0 Likes
7 Replies
MichaelF_56
Moderator
Moderator
Moderator
250 sign-ins 25 comments on blog 10 comments on blog

SDK 2.2.2 has been released to SVT. We are checking to confirm that the test spec includes testing on Windows 10.

0 Likes

Software Verification & Test.

0 Likes
Anonymous
Not applicable

I was able to install the SDK onto the WIN 10.

I downgraded the java to ver 7 U80 and added the path to java bin ( ex: C:\Program File (X86) .../java/jre/bin)  file to the PATH variable. After that I was able to install it on WIN10.

Hope this helps.

0 Likes

Thanks for sharing tejas.kotadia@ubnt.com

Adding a few others that were struggling with the install on Windows 10.

I believe Henryubnt may be a colleague of yours.

joe@openbikeinc  henryubnt  aneedles

0 Likes
Anonymous
Not applicable

Hi mwf_mmfae,

Thank you for connecting us. I have a successful SDK 2.2.1 in Linux and I don't want to spend time to try it again. All I have to do now is just wait for the SDK 2.2.2 for which you mentioned it solved the issue of my project.

Thanks.

0 Likes