- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello everyone.
I have the following problem.
When I put in the code blecen_Scan the timer 1s stopped working.
Has anyone ever had a similar problem?
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Ok, perhaps now I understand the question. If you initiate the blecen_scan in the create function, it will enter this state of scanning until it is interrupted. You will have to implement the blecen_scan(No scan) some where to interrupt/break it, then those timers will continue to work and count. Alternatively, don't start the scan in the create function, put it in an interrupt handler.
For example:
void app_create(void)
{
bleprofile_Init(bleprofile_p_cfg);
bleprofile_GPIOInit(bleprofile_gpio_p_cfg);
// Enable Button Interrupt
// register to process peripheral advertisements, notifications and indications
blecm_RegleAdvReportCb((BLECM_FUNC_WITH_PARAM) advertisement_handler);
blecen_Scan(NO_SCAN);
bleprofile_regTimerCb(app_fine_timer, app_timer);
bleprofile_StartTimer();
}
void app_fine_timer(UINT32 arg){} //do nothing
void app_timer(UINT32 arg){
ble_trace0("1s has elapsed");
}
The above will allow the timer to run, and if I apply an interrupt, the state will change to that of scanning. You may also want to implement a
callback when the scanning process ends, then the device will return to counting again. Insert some traces to show the executions.