Hello,
SDK:2.1.1
Hardware:Tag board + iPhone
I want to send variable data from client(iPhone) to the tag-board.
I have checked some samples and documents, and I found a description of setting "LEGATTDB_PERM_VARIABLE_LENGTH" in MMP920732SW-AN103-R application note, P12, table2.
Does any body know how to set this setting?
The samples just have the setting function CHARACTERISTIC_UUID128_WRITABLE () for write characteristic, and it need the length information like this.
CHARACTERISTIC_UUID128_WRITABLE (HDLC_VSP_VSP_TX,
HDLC_VSP_VSP_TX_VALUE,
__UUID_VSP_VSP_TX,
LEGATTDB_CHAR_PROP_WRITE_NO_RESPONSE,
LEGATTDB_PERM_WRITE_CMD,
16), ect...
It sets the data length, so the length is always 16 or something even iPhone sent other length data.
I want to like this,
When I sent data
0x00 0x00
then I want to get two byte of 0x00.
When I sent
0x00 0x00 0x00
then I want to get three byte of 0x00.
I changed the setting LEGATTDB_PERM_WRITE_CMD to LEGATTDB_PERM_VARIABLE_LENGTH.
I want to get 16byte data paket, so I can not add a length data in the data.
Solved! Go to Solution.
I believe you already asked a similar question here: Characteristic of variable-length write
We have a meeting with the developers this week and will discuss, then respond to the original thread.
I believe you already asked a similar question here: Characteristic of variable-length write
We have a meeting with the developers this week and will discuss, then respond to the original thread.