Hello,
During debug, my WICED Sense2 became a brick.
I tried to recover with WICED Sense Recovery Procedure Video.
However I can't find a boot button on the board and following recover command fails.
wiced_sense2-BCM920737TAG_Q32 recover UART=COMxx
**** Recovery failed - retry ****
How can I recover WICED Sense2?
Best regards,
Nori Shinozaki
Solved! Go to Solution.
Download a copy of the wiced sense 2 FW from the below link:
Then try this:
1) Press and hold "Reset"
2) Insert USB cable
3) Ensure the two usb-to-serial ports are displayed under Device_Manager\Ports
4) Release "Reset"
5) Do a CLEAN before you compile and download
I used "wiced_sense-BCM920737TAG_Q32 recover UART=COM26" on a sense_2 kit.
Adding btta
Download a copy of the wiced sense 2 FW from the below link:
Then try this:
1) Press and hold "Reset"
2) Insert USB cable
3) Ensure the two usb-to-serial ports are displayed under Device_Manager\Ports
4) Release "Reset"
5) Do a CLEAN before you compile and download
I used "wiced_sense-BCM920737TAG_Q32 recover UART=COM26" on a sense_2 kit.
Thanks, it worked!
Nori Shinozaki
"Reset" is the little hole at the back of the dongle, and you will need a needle or safety-pin to press-and-hold a little button in the package.