Hello Everyone,
I have created a simple 5 page PDF with numerous screenshots that walk you through how to do an OTA update with the BCM2073x/BCM2073xS device and the Broadcom SDK. One key thing that I learned sometime back after having OTA's fail ~30% of the time was a simple trick that solves this problem which is to simply UNCHECK the 'Allow the computer to turn off this device to save power' in the USB Dongle/BCM20702 Bluetooth Device Properties tab under Power Management. This is HIGHLY recommended for anyone that plans to make use of OTA updates from a PC using the 20702 + WIDCOMM BTLE stack. PDF and screenshot of this setting are below...
Regards,
Frank
Its helpful !
helpfull
Do you have an example of the bluetooth dongle mentioned in step 5? A specific one i can buy to use
There's a list of BCM20702 based dongles referenced here: Re: Interested in using Broadcom’s Windows stack for Windows 7?