cancel
Showing results for 
Search instead for 
Did you mean: 

Smart Bluetooth

Anonymous
Not applicable

Hi,

Adjust the TX power level

I just see the blecm_setTxPowerInADV() in the SDK2.X.X. Is there any function which like blecm_setTxPowerInConnection() in the SDK2.X.X.

Thanks

ChienYi

0 Likes
1 Solution
ArvindS_76
Employee

> Where could I find out the blecm_setTxPowerInConnection() in SDK2.x.x?

See blecm.h


> blecm_setTxPowerInConnection(): it means that we can modify the TX power in connection mode.

> blecm_setTxPowerInADV(): It means that we can modify the TX power in Advertising mode.

> Is it right?

Yes.

View solution in original post

4 Replies
ShawnA_01
Employee

Hi ChienYi,

Is this forum entry the same as the one you posted over here?  Adjust the TX power level

If not, please re-state the question.

Thanks.

0 Likes
Anonymous
Not applicable

Hi Shawn,

Yes, it is the same forum entry.

We can find out the following functions in the SDK1.x.x.

a.blecm_setTxPowerInConnection()

b.blecm_setTxPowerInADV()


But we only find out the function in the SDK2.x.x.

b.blecm_setTxPowerInADV()


Question:

1. Where could I find out the blecm_setTxPowerInConnection() in SDK2.x.x?

2. blecm_setTxPowerInConnection(): it means that we can modify the TX power in connection mode.

    blecm_setTxPowerInADV(): It means that we can modify the TX power in Advertising mode.

    Is it right?

Thanks

ChienYi

0 Likes
ArvindS_76
Employee

> Where could I find out the blecm_setTxPowerInConnection() in SDK2.x.x?

See blecm.h


> blecm_setTxPowerInConnection(): it means that we can modify the TX power in connection mode.

> blecm_setTxPowerInADV(): It means that we can modify the TX power in Advertising mode.

> Is it right?

Yes.

View solution in original post

Anonymous
Not applicable

Hi Arvinds,

Thanks for your reply.

Thanks

ChienYi

0 Likes