- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Sir ,
I have six 20737s devices and use 2.2.1 sdk.
I look "hello_client" project , it define a variable
#define HELLO_CLIENT_MAX_SLAVES | 4 |
and look "puart_control" project , it define a variable
#define PUART_CONTROL_MAX_CONNECTIONS | 8 |
I use puart_control project do actual test , Max can connections only four ,
When I try to connect a fifth device , the debug port display "connection failure" ,
Really can support connections to eight devices?
thanks you !
Solved! Go to Solution.
- Labels:
-
MasterSlave
-
SDK 2.X
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
puart_control is probably missing a call to set the max number of slaves to 8. Try adding:
blecm_setmaxconnection(PUART_CONTROL_MAX_CONNECTIONS);
to APPLICATION_INIT()
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I think you need to change HELLO_CLIENT_MAX_SLAVES
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi kwang
I use puart_control project
PUART_CONTROL_MAX_CONNECTIONS 8
but it only can connect four devices
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Sorry I misread your post,
Are you using the WICED Sense kits? or your own custom board?
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
Do all your evaluations on the tag3 board. The max number of slaves can be set up to 7. If you include the master, then it will be a total of 8 members in the piconet.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi boont
But I do actual test , a master can only connection four slaves ,limit.
Have you actually measured ?
hello_client project some code in "connection_up" event method :
if (con_index >= HELLO_CLIENT_MAX_SLAVES) // con_index = (0x40 ~ 0x43) - (0x40) , can connect four devices
{
....
return;
}
puart_control project some code in "connection_up" event method ::
if (con_index > PUART_CONTROL_MAX_CONNECTIONS) // The same situation as above
{
.....
return;
}
PUART_CONTROL_MAX_CONNECTIONS is 8 , but actual test only connected four devices (0x40~0x43).
Connect handle no more than 0x43 , because when I try connect fifth slave device , the first debuger port print "connection failure" .
After connected four devices, used bleprofile_Discoverable() method can't Advertising.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Note that we confirmed today with the Developers that the 20737/36 will support up to 8 slaves (i.e. it will be the master of all the 8 slaves).
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
have anyone try use puart_control App connect more than four slave devices ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Maybe I description is not clear enough.
I step by step do to you look :
step 1:
Scan result of five 20737 chip device:
step 2:
Connect address :0x1234567890DD
step 3:
Connect address :0x1234567890CC
Step 4 :
Connect address :0x1234567890AA
Step 5 :
Connect address :0x1234567890EE
Step 6:
I finish connect four slave devices ,I try connect 5th device 0x1234567890BB slave devices,
but can't connect it , no any connect success message !
step 7 :
final I click start advertisements , I use ble sinffer , not catch any package about this device.
and slave device 0x1234567890BB still advertisements !
-------------------------------------------------------------------------------------------------------------------------------------------------
Really can connect more than four slave devices ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
puart_control is probably missing a call to set the max number of slaves to 8. Try adding:
blecm_setmaxconnection(PUART_CONTROL_MAX_CONNECTIONS);
to APPLICATION_INIT()
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi thanks you ,
I add this function blecm_setmaxconnection(PUART_CONTROL_MAX_CONNECTIONS);
it slove my problem !
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
yaocing_shih is this still an issue?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi kwang !
Sorry Answer delay !
I No problem now.
Thank you for your interest