- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi,
I found some functions in WICED, ble_tracex(), which are similar with printf().
So I want to know that how can I use ble_tracex() function to debug application through HCI uart port? If so, it will be good for application development.
Regards,
Kai Ren
Solved! Go to Solution.
- Labels:
-
Debug
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
In your APPLICATION_INIT() function, if you set ble_trace_enable = 1, ble_trace* functions will print to the peripheral UART. If you set this to 2 instead, debug traces will go to the HCI UART. Since the 20732 ROM uses HCI UART RXd to detect the presence of a host device (for download mode), make sure that you disconnect RXd line, leaving the TXd line connected and then power cycle the device (or the device will enter download mode again).Setting ble_trace_enable = 0 instead will disable all debug messages.Hi,I want to set ble_trace_enable = 1, to use puart port as debug port. But the result is nothing. When I send some words to BCM20732_TAG, it echo these words back. Baud rate is 57600.Do I need to initial puart or do some extra action for puart? Kaiser

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi,I found some functions in WICED, ble_tracex(), which are similar with printf().So I want to know that how can I use ble_tracex() function to debug application through HCI uart port? If so, it will be good for application development.Regards,Kai RenTake a look at this post here and see if it answers your question Kai: http://forum.broadcom.com/showthread.php?91088-Information-BCM20732S-debug-trace-capabilities-throug...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi mwf_mmfae:
I had the same question with Kai.
I had try to access
" Take a look at this post here and see if it answers your question Kai:http://forum.broadcom.com/showthread.php?91088-Information-BCM20732S-debug-trace-capabilities-throug...
but I got :
Message
Roger Wang, you do not have permission to access this page. This could be due to one of several reasons:
- Your user account may not have sufficient privileges to access this page. Are you trying to edit someone else's post, access administrative features or some other privileged system?
- If you are trying to post, the administrator may have disabled your account, or it may be awaiting activation.
How to do set the ble_trace_enable=2 ?
Thanks
Roger Wang
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi mwf_mmfae:
I had find out :
extern UINT8 bleapp_trace_enable;
in bleprofile.h
that is the same ble_trace_enable ?
May I use this bleapp_trace_enable=2 for debug my firmware ?

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
The link above goes to the website where the forums were hosted originally. These were moved to the current site 14 months ago.
That thread specifically is here: Information: BCM20732S debug/trace capabilities through the HCI UART port
Note that while ble_trace_enable can be used on this manner to direct traces, there is a new method which is easier to use and described within the WICED Smart Quick Start Guide (SDK 1.x and TAG2 Board)
I linked to the Quick Start guide which refers to the 20732 and TAG1 board as that appears to be what you are using.
The Quick Start guide here is for the A1 20736/37 and the newer TAG3 board: WICED Smart Quick Start Guide (SDK 2.x and TAG3 Board)
The Quick Start guide is a great source for setting up traces on the older chip/TAG board.

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi,I want to set ble_trace_enable = 1, to use puart port as debug port. But the result is nothing. When I send some words to BCM20732_TAG, it echo these words back. Baud rate is 57600.Do I need to initial puart or do some extra action for puart? KaiserWhat is your applications BLE_PROFILE_PUART_CFG? By default, the baud rate for BRCM sample applications is set to 115200. Have you hooked up your terminal application to the GPIOs in this configuration?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
What is your applications BLE_PROFILE_PUART_CFG? By default, the baud rate for BRCM sample applications is set to 115200. Have you hooked up your terminal application to the GPIOs in this configuration?This is BLE_PROFILE_PUART_CFG in proximity_plus.c, I have defined BLEDEBUG. So, P32 and P33 are puart pin.PLACE_IN_DROM const BLE_PROFILE_PUART_CFG bleprox_mod_puart_cfg ={ /*.baudrate =*/ 115200, #ifdef BLEDEBUG /*.txpin =*/ 32, //20730A0 module need to use 32 instead, normally it is 31 /*.rxpin =*/ 33, //GPIO pin number#else /*.txpin =*/ PUARTDISABLE | 32, /*.rxpin =*/ PUARTDISABLE | 33, #endif};On schematic, I found that U11s pin1 and pin2 are connected with P32 and P33, then I solid out two wire and use http://www.ftdichip.com/Products/Cables/USBTTLSerial.htm this type of usb2rs232 cable to monitor puart port.BTW, I dont know how to hook up the terminal application to the GPIOs.[ATTACH=CONFIG]177[/ATTACH]
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
Hello Kai.ren,I apologize for the delay in getting back to you.Based on the photo you attached, I think I see what the problem is you are having jumpering to P33(Pin 24 on the chip, PUART_RX) and P32(Pin 25 on the chip, PUART_TX) coming off leads from the unused serial flash located in U11.If you take a look at the schematic, R100 and R101 are DNI. Since it appears from the photo you provided that you are jumpering off the leads on the serial flash itself, there is no connection either to P33 or P32.What you want to try is to solder your leads in the same manner on the side of the ball allocated to the DNI resistors that is closest to the BCM20732.Hi,A low level mistake, sorry.I have installed two 0Ohm resistors on R100 and R101, instead of your method, sold leads from the closest pot of BCM20732. It can printf some strings.Thanks,BTW, does my method have any side effect?

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content