Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
StDa_4617271
Level 1
Level 1

Good morning, I tried to enable CYBT343026 bluetooth module by HCI Uart commands, but I can't see it trought bluetooth of my smartphones.

To send commands to BT module I use CyBlueTool.

I've enabled radio, set tx power, assigned name to device and bd_addr, but without success.

What did I forget?

Thanks in advance for your help.

Regards

0 Likes
1 Solution
SheetalJ
Moderator
Moderator
Moderator
First comment on KBA 750 replies posted 500 likes received

Hi StDa_4617271​,

Can you please check if reset command is giving a success in CyBluetool logs? Make sure you have opened HCI COM port in CyBluetool. If reset shows success, then try sending 'read BD_address' command and check if you can see device BD address in your logs.

If yes, then you can send start advertising command and try scanning device in your smartphone.

View solution in original post

0 Likes
5 Replies
DheerajPK_41
Moderator
Moderator
Moderator
750 replies posted 500 likes received 500 replies posted

Hi,

Could you please share the cybluetool log with us? (copy paste the log into text file and attach in your response here).

We will check and let you know where the fail happened, and how to overcome it.

Thanks,

-Dheeraj

Hi, here the log:

07/24/20 08:51:43.573 com10 -- Transport opened

com10@115200

07/24/20 08:51:43.573 com10 -- Protocol set to HCI

com10@115200

07/24/20 08:51:43.590 com10@115200 c> LE_Read_Buffer_Size_v2

HCI Command

com10@115200

[60 20 00 ]

opcode = 0x2060 (8288, "LE_Read_Buffer_Size_v2")

07/24/20 08:51:43.623 com10 <c LE_Read_Buffer_Size_v2

HCI Command Complete Event

com10@115200

[0E 04 ]: 01 60 20 01

event = 0x0E (14,"Command Complete")

Num_HCI_Command_Packets = 0x1 (1)

Command_Opcode = 0x2060 (8288, "LE_Read_Buffer_Size_v2")

Status = 0x1 (1, "Unknown HCI Command", "Unknown HCI Command")

07/24/20 08:51:57.538 com10@115200 c> Reset

HCI Command

com10@115200

[03 0C 00 ]

opcode = 0x0C03 (3075, "Reset")

07/24/20 08:51:57.585 com10 <c Reset

HCI Command Complete Event

com10@115200

[0E 04 ]: 01 03 0C 00

event = 0x0E (14,"Command Complete")

Num_HCI_Command_Packets = 0x1 (1)

Command_Opcode = 0xC03 (3075, "Reset")

Status = 0x0 (0, "Success", "Success")

07/24/20 08:52:07.013 com10@115200 c> Read_BD_ADDR

HCI Command

com10@115200

[09 10 00 ]

opcode = 0x1009 (4105, "Read_BD_ADDR")

07/24/20 08:52:07.059 com10 <c Read_BD_ADDR

HCI Command Complete Event

com10@115200

[0E 0A ]: 01 09 10 00 FF FF FF FF FF FF

event = 0x0E (14,"Command Complete")

Num_HCI_Command_Packets = 0x1 (1)

Command_Opcode = 0x1009 (4105, "Read_BD_ADDR")

Status = 0x0 (0, "Success", "Success")

BD_ADDR = "FFFFFFFFFFFF"

07/24/20 08:52:36.775 com10@115200 c> LE_Set_Advertise_Enable

HCI Command

com10@115200

[0A 20 01 ]: 01

opcode = 0x200A (8202, "LE_Set_Advertise_Enable")

Advertising_Enable = 0x1 (1, "Advertising is enabled")

07/24/20 08:52:36.787 com10 <c LE_Set_Advertise_Enable

HCI Command Complete Event

com10@115200

[0E 04 ]: 01 0A 20 00

event = 0x0E (14,"Command Complete")

Num_HCI_Command_Packets = 0x1 (1)

Command_Opcode = 0x200A (8202, "LE_Set_Advertise_Enable")

Status = 0x0 (0, "Success", "Success")

07/24/20 08:54:14.313 com10@115200 c> Write_BD_ADDR

HCI Command

com10@115200

[01 FC 06 ]: FF EE DD CC BB AA

opcode = 0xFC01 (64513, "Write_BD_ADDR")

BD_ADDR = "AABBCCDDEEFF"

07/24/20 08:54:14.321 com10 <c Write_BD_ADDR

HCI Command Complete Event

com10@115200

[0E 04 ]: 01 01 FC 00

event = 0x0E (14,"Command Complete")

Num_HCI_Command_Packets = 0x1 (1)

Command_Opcode = 0xFC01 (64513, "Write_BD_ADDR")

Status = 0x0 (0, "Success", "Success")

07/24/20 08:54:20.925 com10@115200 c> Read_BD_ADDR

HCI Command

com10@115200

[09 10 00 ]

opcode = 0x1009 (4105, "Read_BD_ADDR")

07/24/20 08:54:20.957 com10 <c Read_BD_ADDR

HCI Command Complete Event

com10@115200

[0E 0A ]: 01 09 10 00 FF EE DD CC BB AA

event = 0x0E (14,"Command Complete")

Num_HCI_Command_Packets = 0x1 (1)

Command_Opcode = 0x1009 (4105, "Read_BD_ADDR")

Status = 0x0 (0, "Success", "Success")

BD_ADDR = "AABBCCDDEEFF"

07/24/20 08:54:54.781 com10@115200 c> Write_Local_Name

HCI Command

com10@115200

[13 0C F8 ]: 54 45 53 54 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

opcode = 0x0C13 (3091, "Write_Local_Name")

Name = "TEST"

07/24/20 08:54:54.811 com10 <c Write_Local_Name

HCI Command Complete Event

com10@115200

[0E 04 ]: 01 13 0C 00

event = 0x0E (14,"Command Complete")

Num_HCI_Command_Packets = 0x1 (1)

Command_Opcode = 0xC13 (3091, "Write_Local_Name")

Status = 0x0 (0, "Success", "Success")

07/24/20 08:55:15.762 com10@115200 c> Read_Local_Name

HCI Command

com10@115200

[14 0C 00 ]

opcode = 0x0C14 (3092, "Read_Local_Name")

07/24/20 08:55:15.824 com10 <c Read_Local_Name

HCI Command Complete Event

com10@115200

[0E FC ]: 01 14 0C 00 54 45 53 54 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

event = 0x0E (14,"Command Complete")

Num_HCI_Command_Packets = 0x1 (1)

Command_Opcode = 0xC14 (3092, "Read_Local_Name")

Status = 0x0 (0, "Success", "Success")

Name = "TEST"

Thanks for help.

0 Likes

From the logs, I can see that your commands are being successfully executed, showing that your problem is resolved.

0 Likes

Hi, now with this commands I see correctly the module BT:

7.3 RESET

7.3 Write_Local_Name

0   Write_BD_ADDR

0   Enable_Radio

7.8 LE_Set_Advertise_Enable

Thanks.

Best regards.

0 Likes
SheetalJ
Moderator
Moderator
Moderator
First comment on KBA 750 replies posted 500 likes received

Hi StDa_4617271​,

Can you please check if reset command is giving a success in CyBluetool logs? Make sure you have opened HCI COM port in CyBluetool. If reset shows success, then try sending 'read BD_address' command and check if you can see device BD address in your logs.

If yes, then you can send start advertising command and try scanning device in your smartphone.

0 Likes