- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
So with the Glucose Profile I am trying to do a simple read of measurement data …
It seems that before ANY RACP calls can be made you have setup the Client Config for to allow measurement, context etc
So in LightBlue I first start a notify on the 0x2A18 characteristic (ie, measurement), then 0x2A34 (ie, context)
Then on RACP 0x2A52 I write a HEX 0x04 then app asks to be paired and it does not error so I assume it paired
Then I send it a HEX 0x01 and I do see the blebgm_IndicationConf being called but I don’t know where the measurement data should appear on the LightBlue app?
I have already successfully connected the BLE & Meter UARTS and am communicating between them just not sure how to get that glucose data over the Central side of things … my guess is it should be really simple … and should just work
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I think the key to getting the LightBlue app is knowing that one must send the HEX value together ...
I was doing it separately ...
So when I tried "04 01" then I received "0x05006400" which I believe is the correct response of "100" records
Now just need to figure out how dump the glucose readings back to the app ... I hope it's similar
Just need to figure out where all the OpCodes are listed