Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Smart Bluetooth Forum Discussions

ThYo_2228536
Level 3
Level 3
First like received First like given

Recommendation for "future" board to replace  BCM92073X_LE_KIT

1) Pin Header : not convenient at all to wire TP6 for SPI CLOCK and TP7  for MISO in the back of the board to be able to configure SPI in MASTER2_P24_CLK_P04_MOSI_P25_MISO

2) Default voltage of the board is 1.2 V or so. While it is good as a marketing point of view to sell low power BLE using coin cell, it uis not good enough to power SPI slaves.

3) SPI driver in wiced smart is not as good as STM SPI driver today.  WICED WIFI uses STM for SPI and Host MCU.

Using Host MCU for BLE is a good idea but it is not full feature enough to be abke connect with ALL third party devices out there.

I found issues with Analog Device ADC as well as  Linear LTC2983 SPI ADC. All those board are requiring 3.3 V mimimum.

It looked like when trying to power SPI slave through BLE as 3.3 V after HW modification. SPI MISO, CLOCK and MOSI are all screwed up although the 3.3 V modidief board was able to drive the  Aardvark SPI/I2C Atmel Connectivity demo board,

So it looked like a build in level shifter would be needed or some sort.

I am not an hardware engineer but just felt the frustration not beeing able to read anything using SPI master interface after the board was modified for 3.3 V.

Finally I noticed that idevice Connected Devices - Bluetooth Module & Product Development | iDevices LLC is using "iDevices Bluetooth Smart Module from Broadcom" as a platform that can simply connect to their favorite CPU/Micro-controller via a UART interface.

It is interesting that they decided to use UART for iGrill  to have BLE communicate with a bigger Host MCU over UART to exchange data back and forth and let the HOST MCU deal with SPI communciation with Thermocouple and ADC. It looked like it confirms that SPI driver is better on STM today. It is too bad because on paper the BLE should be able to drive 4 SPI slave device.

If Broadcom want to connect everything then the eval board should be able to do so up front. I am affraid it needs to do more so I am looking forward to the next BLE Board!

0 Likes
1 Solution
Anonymous
Not applicable

Hello Thomas,

Thank you for your comments:

Recommendation for "future" board to replace  BCM92073X_LE_KIT

1) Pin Header : not convenient at all to wire TP6 for SPI CLOCK and TP7  for MISO in the back of the board to be able to configure SPI in MASTER2_P24_CLK_P04_MOSI_P25_MISO

[JT] - Thanks for this input.

2) Default voltage of the board is 1.2 V or so. While it is good as a marketing point of view to sell low power BLE using coin cell, it uis not good enough to power SPI slaves.

[JT] - The default voltage of the next TAG board will be 3.3V.

3) SPI driver in wiced smart is not as good as STM SPI driver today.  WICED WIFI uses STM for SPI and Host MCU.

Using Host MCU for BLE is a good idea but it is not full feature enough to be abke connect with ALL third party devices out there.

I found issues with Analog Device ADC as well as  Linear LTC2983 SPI ADC. All those board are requiring 3.3 V mimimum.

[JT] - Our next board will have a prototyping area to accommodate the ADC you mentioned.

I am not an hardware engineer but just felt the frustration not beeing able to read anything using SPI master interface after the board was modified for 3.3 V.

[JT] - No level shifters are needed.  We will take this into consideration on the next TAG board - Thanks

Finally I noticed that idevice Connected Devices - Bluetooth Module & Product Development | iDevices LLC is using "iDevices Bluetooth Smart Module from Broadcom" as a platform that can simply connect to their favorite CPU/Micro-controller via a UART interface.

It is interesting that they decided to use UART for iGrill  to have BLE communicate with a bigger Host MCU over UART to exchange data back and forth and let the HOST MCU deal with SPI communciation with Thermocouple and ADC. It looked like it confirms that SPI driver is better on STM today. It is too bad because on paper the BLE should be able to drive 4 SPI slave device.

[JT] - The SPI ports can drive 2 slave devices.

If Broadcom want to connect everything then the eval board should be able to do so up front. I am affraid it needs to do more so I am looking forward to the next BLE Board!

[JT] - Coming soon!

View solution in original post

5 Replies
Anonymous
Not applicable

Hello Thomas,

Thank you for your comments:

Recommendation for "future" board to replace  BCM92073X_LE_KIT

1) Pin Header : not convenient at all to wire TP6 for SPI CLOCK and TP7  for MISO in the back of the board to be able to configure SPI in MASTER2_P24_CLK_P04_MOSI_P25_MISO

[JT] - Thanks for this input.

2) Default voltage of the board is 1.2 V or so. While it is good as a marketing point of view to sell low power BLE using coin cell, it uis not good enough to power SPI slaves.

[JT] - The default voltage of the next TAG board will be 3.3V.

3) SPI driver in wiced smart is not as good as STM SPI driver today.  WICED WIFI uses STM for SPI and Host MCU.

Using Host MCU for BLE is a good idea but it is not full feature enough to be abke connect with ALL third party devices out there.

I found issues with Analog Device ADC as well as  Linear LTC2983 SPI ADC. All those board are requiring 3.3 V mimimum.

[JT] - Our next board will have a prototyping area to accommodate the ADC you mentioned.

I am not an hardware engineer but just felt the frustration not beeing able to read anything using SPI master interface after the board was modified for 3.3 V.

[JT] - No level shifters are needed.  We will take this into consideration on the next TAG board - Thanks

Finally I noticed that idevice Connected Devices - Bluetooth Module & Product Development | iDevices LLC is using "iDevices Bluetooth Smart Module from Broadcom" as a platform that can simply connect to their favorite CPU/Micro-controller via a UART interface.

It is interesting that they decided to use UART for iGrill  to have BLE communicate with a bigger Host MCU over UART to exchange data back and forth and let the HOST MCU deal with SPI communciation with Thermocouple and ADC. It looked like it confirms that SPI driver is better on STM today. It is too bad because on paper the BLE should be able to drive 4 SPI slave device.

[JT] - The SPI ports can drive 2 slave devices.

If Broadcom want to connect everything then the eval board should be able to do so up front. I am affraid it needs to do more so I am looking forward to the next BLE Board!

[JT] - Coming soon!

Anonymous
Not applicable

Isn't it at least theoretically possible to drive many slave devices using the single SPIFFY2 interface by using the CS (Chip Select) lines on the slave devices to select which one you want to control at any given time?

I would like to resoundingly second the motion on #1 and #2 above.  Trying to drive a 3.3v CMOS ADC chip from Texas Instruments with the TAG proved quite challenging, and I have yet to complete that project.  hmm.  maybe I can work on that today while I wait for my new programming cables to arrive...

Speaking of programming cables, PLEASE CHANGE THE MOLEX JP1 connector on the TAG board to something larger and more common... or provide a cable accessory that mates with it.  It was not easy to find a cable for this and I ended up having a custom cable made.

To re-iterate...

1. Maybe some jumpered voltage options for the TAG would be nice, but 3.3 volts will do.  The fixed voltage is very limiting.

2. I found the only SPIFFY2 ports available for use were solder pads on the back of the board.  thank you for providing additional header pins for these in the future.

3. JP1 needs to be bigger and easier to work with.  Don't worry about making the TAG small... it's a development tool, and smaller is harder to see and to work with.  My eyes aren't as good as they used to be.

ehoffman: Which TI board are you planning to use ?

jt: please let me know when a new board is available and please ship one to my attention

0 Likes

- Don't worry about making the TAG small...

Well best of both world please. Having a small tag is good for prototyping when you want to build a case to hold

all the boards and wire together. This would be great to post some 3D printing model for WICED   for  stratasys mojo printer to print your own casin and recommend some casing from http://www.digikey.com/product-search/en?lang=en&site=us&keywords=enclosures&x=0&y=0

Final product disign and look and feel even for prototype is very important too !

0 Likes
Anonymous
Not applicable

Thanks for the feedback, Thomas!

JT

0 Likes