- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Is there any recommendation provided by Broadcom for the SW that should be used to pass the FCC certification for the BCM20736S?
Is there a Test Suite that will be provided by Broadcom that can be used during the FCC certification work? Something that would cover BLE stress test or specific scenarios?
Solved! Go to Solution.
- Labels:
-
Manufacturing and Test
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
The Manufacturing Bluetooth test tool (MBT) will be introduced in SDK 2.1 and can be used to test and verify the RF performance of the BCM2073x family of SoC Bluetooth Low Energy (BLE) devices.
Each test essentially sends an HCI command to the device and then waits for an HCI Command Complete event from the device.
The following tests will be available using this tool:
- Reset Test
- LE Receiver Test
- LE Transmitter Test
- LE Test End
- Continuous Transmit Test
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
The Manufacturing Bluetooth test tool (MBT) will be introduced in SDK 2.1 and can be used to test and verify the RF performance of the BCM2073x family of SoC Bluetooth Low Energy (BLE) devices.
Each test essentially sends an HCI command to the device and then waits for an HCI Command Complete event from the device.
The following tests will be available using this tool:
- Reset Test
- LE Receiver Test
- LE Transmitter Test
- LE Test End
- Continuous Transmit Test
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Excellent, thanks for listing the detail of the tests.