- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi all,
I'm using the 20736's random number generator and I seem to be getting some repeated numbers once in a while (but more often than expected).
I'm wondering if it's a pseudo-random number generator (software, needs manual seeding), instead of a hardware one (which does self-seeding).
The problem is really when, for example, I use 1000 different devices to generate their own 32-bit ID numbers. When the central retrieves their IDs, we noticed that some ID numbers were generated by a few devices.
Example:
Id 0x12345678 only 1 device
...
Id 0x9ABCDEF only 1 device
...
Id 0x34FE0207 was generated by 4 devices
...
Id 0xFF810ADD was generated by 3 devices
...
etc
In the end, the central reported that there only about 700 unique IDs among those 1000 devices.
Is this an expected limitation or am I doing something wrong?
Here's what I did:
UINT32 random_number;
ulp_rand(&random_number, 1);
Thanks!
Gil
Message was edited by: Guilherme de Paula
Solved! Go to Solution.
- Labels:
-
Security
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Guilherme,
Yes, it is a true HW Random Number generator.
You will need to wait until 500ms after boot in order to use the HW RNG.
Hope this helps.
Thanks
JT