Does anyone have an example how to use the UART on the WICED Sense Kit?

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hi,

Is there an example somewhere illustrating how to use the UART ?

From what I read the UART is associated with P32/P33 whihc are connected to the standard serial port of the USB. Hence this would be perfect to output some debug message or information.

0 Likes
1 Solution
Anonymous
Not applicable

Hello Benoit,

Yes, you are correct in the P-UART USB use case.  Our TAG003 development board allows Switch settings to enable the P_UART as a debug port.

The WICED Sense Kit was introduced for the Hackathon as a Pre-Production device and the P_UART was not enabled.

Thanks

JT

View solution in original post

3 Replies
Anonymous
Not applicable

Hello Benoit,

Yes, you are correct in the P-UART USB use case.  Our TAG003 development board allows Switch settings to enable the P_UART as a debug port.

The WICED Sense Kit was introduced for the Hackathon as a Pre-Production device and the P_UART was not enabled.

Thanks

JT

Anonymous
Not applicable

Hi j.t.

Thanks for your response. So you mean trhe device we have has a failure and there is no way use the UART. Hence no real way to debug the code we would write to run on the wiced_sense ?

Thanks,

Benoit.

0 Likes
Anonymous
Not applicable

Hi bchristi

not sure if you already found an answer, but for all readers like me that are new into this and searching in the forum before posting, here are some links to the answer:

WICED Sense debug with UART

And further details and example :

WICED Sense debug with UART (continued)

Wassim

0 Likes