- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Overview
On WICED Smart device, the default advertising data includes Flags,Local Name, Class of Device and Service UUID, etc. Developer can customize the advertising data, this document introduce how to make a customized advertising.
Advertising Data Format
The format of advertising data is shown in the follow figure. The data consist of a significant part and a non-significant part. The significant part contains a sequence of AD structure, the non-significant part extends the advertising to 31 octets and shall contain all-zero octets.
Advertising Data Type
About AD type definition, please refer to https://www.bluetooth.org/en-us/specification/assigned-numbers/generic-access-profile .
The following AD types are defined in SDK, it’s in bleprofile.h.
// ADV flag values
enum ble_adv_flag_value
{
ADV_FLAGS = 0x01,
ADV_SERVICE_UUID16_MORE = 0x02,
ADV_SERVICE_UUID16_COMP = 0x03,
ADV_SERVICE_UUID32_MORE = 0x04,
ADV_SERVICE_UUID32_COMP = 0x05,
ADV_SERVICE_UUID128_MORE = 0x06,
ADV_SERVICE_UUID128_COMP = 0x07,
ADV_LOCAL_NAME_SHORT = 0x08,
ADV_LOCAL_NAME_COMP = 0x09,
ADV_TX_POWER_LEVEL = 0x0A,
ADV_CLASS_OF_DEVICE = 0x0D,
ADV_SIMPLE_PAIRING_HASH_C = 0x0E,
ADV_SIMPLE_PAIRING_RANDOMIZER_R = 0x0F,
ADV_TK_VALUE = 0x10,
ADV_OOB_FLAGS = 0x11,
ADV_SLAVE_CONNECTION_INTERVAL_RANGE = 0x12,
ADV_SERVICE_UUID16 = 0x14,
ADV_SERVICE_UUID128 = 0x15,
ADV_SERVICE_DATA = 0x16,
ADV_SERVICE_TARGET_PUBLIC_ADR = 0x17,
ADV_SERVICE_TARGET_RANDOM_ADR = 0x18,
ADV_APPEARANCE = 0x19,
ADV_ADVERTISING_INTERVAL = 0x1A,
ADV_3D_INFORMATION_DATA = 0x3D,
ADV_MANUFACTURER_DATA = 0xFF,
};
Flags
Refer to Core Spec V4.0 [Vol.3], Part C Section 18.1.
Value | Description | Bit | Information |
0x01 | Flags | 0 | LE Limited Discoverable Mode |
1 | LE General Discoverable Mode | ||
2 | BR/EDR Not Supported | ||
3 | Simultaneous LE and BR/EDR to Same Device Capable (Controller) | ||
4 | Simultaneous LE and BR/EDR to Same Device Capable (Host) | ||
5..7 | Reserved |
Service UUIDs
Refer to Core Spec V4.0 [Vol.3], Part C Section 18.2.
A device may list the service UUIDs that it implements in its advertising data.
Value | Description | Information |
0x02 | 16-bit Service UUIDs | More 16-bit UUIDs available |
0x03 | 16-bit Service UUIDs | Complete list of 16-bit UUIDs available |
0x04 | 32-bit Service UUIDs | More 32-bit UUIDs available |
0x05 | 32-bit Service UUIDs | Complete list of 32-bit UUIDs available |
0x06 | 128-bit Service UUIDs | More 128-bit UUIDs available |
0x07 | 128-bit Service UUIDs | Complete list of 128-bit UUIDs available |
Local Name
Refer to Core Spec V4.0 [Vol.3], Part C Section 18.3.
The Local Name ADtype contains the device name, either complete or shortened. If the name is shortened, the complete device name can be read by reading the device name characteristic.
Value | Description | Information |
0x08 | Local Name | Shortened local name |
0x09 | Local Name | Complete local name |
Tx Power Level
Refer to Core Spec V4.0 [Vol.3], Part C Section 18.4.
The TX PowerLevel AD type indicates the transmitted power level of the advertising packet.
Value | Description | Information |
0x0A | TX Power Level (1 byte) | 0xXX:-127 to +127dBm Note: when the TX Power Level tag is not present, the TX power level of the packet is unknown. |
Class of Device
Refer to Core Spec V4.0 [Vol.3], Part C Section 18.5.
Value | Description | Information |
0x0D | Class of device (3 octets) | Format defined in Assigned Numbers. Assigned Numbers Specification: https://www.bluetooth.org/Technical/AssignedNumbers/home.htm |
Simple Pairing Hash C-192
Refer to Core Spec V4.0 [Vol.3], Part C Section 18.5.
Value | Description | Information |
0x0E | Simple Pairing Hash C (16 octets) | Format defined in Core Spec V4.0 [Vol. 2], Part H Section 7.2.2 |
Simple Pairing Randomizer R-192
Refer to Core Spec V4.0 [Vol.3], Part C Section 18.5.
Value | Description | Information |
0x0F | Simple Pairing Randomizer R (16 ctets) | Format defined in Core Spec V4.0 [Vol. 2], Part H Section 7.2.2 |
Security Manager TK Value
Refer to Core Spec V4.0 [Vol.3], Part C Section 18.6.
The Security Manager TK Value only be used over an out-of-band mechanism,the definition as below.
Value | Description | Information |
0x10 | TK Value | Value as used in pairing over LE Physical channel. Format defined in Core Spec V4.0 [Vol. 3], Part H Section 2.3 |
Security Manager Out of Band (OOB)
Refer to Core Spec V4.0 [Vol.3], Part C Section 18.7.
An out of bandmechanism is used by the Security Manager to communicate discovery information as well as other information related to the pairing process.
Value | Description | Bit | Information |
0x11 | Flag (1 octet) | 0 | OOB Flags Field (0 = OOB data not present, 1 = OOB data present) |
1 | LE supported (Host) (i.e. bit 65 of LMP Extended Feature bits Page 1 | ||
2 | Simultaneous LE and BR/EDR to Same Device Capable (Host) (i.e. bit 66 of LMP Extended Feature bits Page 1) | ||
3 | Address type (0 = Public Address, 1 = Random Address) | ||
4..7 | Reserved |
Slave Connection Interval Range
Refer to Core Spec V4.0 [Vol.3], Part C Section 18.8.
The Slave Connection Interval Range AD type contains the Peripheral’s preferred connection interval range, for all logical connections.
Value | Description | Information |
0x12 | Slave Connection Interval Range | The first 2 octets defines the minimum value for the connection interval in the following manner:
Conn_Interval_Min range: 0x0006 to 0x0C80 Value of 0xFFFF indicates no specific minimum. Values outside the range are reserved. (excluding 0xFFFF) The second 2 octets defines the maximum value for the connection interval in the following manner: connInterval_max= Conn_Interval_Max * 1.25 ms Conn_Interval_Max range: 0x0006 to 0x0C80 Conn_Interval_Max shall be equal to or greater than the onn_Interval_Min. Value of 0xFFFF indicates no specific maximum. Values outside the range are reserved (excluding 0xFFFF) |
Service Solicitation
Refer to Core Spec V4.0 [Vol.3], Part C Section 18.9.
One of the Service Solicitation AD types may be sent to invite other devices that expose one or more of the services specified in the Service Solicitation data to connect. This enables a Central providing one or more of these services to connect to this Peripheral.
Value | Description | Information |
x14 | Service UUIDs | List of 16 bit Service UUIDs |
0x15 | Service UUIDs | List of 128 bit Service UUID |
Service Data
Refer to Core Spec V4.0 [Vol.3], Part C Section 18.10.
The Service Data AD type consists of a service UUID with the data associated with that service.
Value | Description | Information |
0x16 | Service Data (2 or more | The first 2 octets contain the 16 bit Service UUID followed by additional service data |
Public Target Address
Refer to Supplement to Core Spec V4.0, Part A Section 1.13.
The public device address is divided into the following two fields:
• company_assigned field is contained in the 24 least significant bits
• company_id field is contained in the 24 most significant bits
Value | Description |
0x17 | Size: Multiples of 6 octets The format of each 6 octet address is the same as the Public Device Address defined in Core Spec V4.0 [Vol. 6], Part B, Section 1.3. The Public Target Address value shall be the enumerated value as defined by Bluetooth Assigned Numbers. Assigned Numbers Specification: https://www.bluetooth.org/Technical/AssignedNumbers/home.htm |
Random Target Address
Refer to Supplement to Core Spec V4.0, Part A Section 1.14.
The random device address is divided into the following two fields:
• hash field is contained in the 24 least significant bits, as defined in [Vol. 3] Part C, Section 10.8.2.3.
• random field is contained in the 24 most significant bits, as defined in [Vol. 3] Part C, Section 10.8.2.2.
Value | Description |
0x18 | Size: Multiples of 6 octets The format of each 6 octet address is the same as the Random Device Address defined in Core Spec V4.0 [Vol. 6], Part B, Section 1.3. The Random Target Address value shall be the enumerated value as defined by Bluetooth Assigned Numbers. Assigned Numbers Specification: https://www.bluetooth.org/Technical/AssignedNumbers/home.htm |
Appearance
Refer to Supplement to Core Spec V4.0, Part A Section 1.12.
Value | Information |
0x19 | The Appearance value shall be the enumerated value as defined by Bluetooth Assigned Numbers. Assigned Numbers Specification: https://www.bluetooth.org/Technical/AssignedNumbers/home.htm |
Advertising Interval
The advertising Interval shall be an integer multiple of 0.625ms in the range of 20ms to 10.24s.
If the advertising event type is either a scannable undirected event type or a non-connectable undirected event type, the advertising Interval shall not be less than 100ms. If the advertising event type is a connectable undirected event type, the advertising Interval can be 20ms or greater.
Value | Information |
0x1A | Size: 2 octets (UINT16) Units: 0.625ms |
Manufacturer Specific Data
Refer to Core Spec V4.0 [Vol.3], Part C Section 18.11.
The Manufacturer Specific AD type is used for manufacturer specific data.
Value | Description | Information |
0xFF | Manufacturer Specific Data (2 or more octets) | The first 2 octets contain the Company Identifier Code followed by additional manufacturer specific data |
Sample Code
The follow sample code is in hello_sensor.c.
void hello_sensor_create(void)
{
…
// Read value of the service from GATT DB.
bleprofile_ReadHandle(HANDLE_HELLO_SENSOR_SERVICE_UUID, &db_pdu);if (db_pdu.len != 16)
{
ble_trace1("hello_sensor bad service UUID len: %d\n", db_pdu.len);
}
else
{
BLE_ADV_FIELD adv[3];//Advertising data type: Flags
adv[0].len = 1 + 1;
adv[0].val = ADV_FLAGS;
adv[0].data[0] = LE_LIMITED_DISCOVERABLE | BR_EDR_NOT_SUPPORTED;//Advertising data type: service UUIDs
adv[1].len = 16 + 1;
adv[1].val = ADV_SERVICE_UUID128_COMP;
memcpy(adv[1].data, db_pdu.pdu, 16);//Advertising data type: Name
adv[2].len = strlen(bleprofile_p_cfg->local_name) + 1;
adv[2].val = ADV_LOCAL_NAME_COMP;
memcpy(adv[2].data, bleprofile_p_cfg->local_name, adv[2].len - 1);//Generate the advertising packet by above three data types
bleprofile_GenerateADVData(adv, 3);
}//Start to advertising
bleprofile_Discoverable(HIGH_UNDIRECTED_DISCOVERABLE, hello_sensor_remote_addr);
}
- Tags:
- advertising data format
- advertsing
- custom advertising
- custom packet
- modify advertising
- packets
- teaser

- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Hi All,
Welcome your comments.