Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Smart Bluetooth Forum Discussions

Anonymous
Not applicable

Hi everyone,

I was curious about the actual current draw and duration of an advertisement on the WICED Sense board with the 20737S chip so I did some testing and thought I'd share since I couldn't find any similar information on the forums. Tests were done with only advertising, no scanning.

Current is calculated by measuring the voltage over a known resistance of 10 ohms in the power path.

I found that given a normal ADV packet size (shown below) and an advertising interval of 100ms, the device drew approximately 25mA of current during the advertisement event for a duration of approximately 2.5ms. It drew roughly 4.5mA on average.

Typical ADV packet setup and payload

// total length should be less than 31 bytes

BLE_ADV_FIELD adv[4];  // advertisement

// flags

adv[0].len    = 1 + 1;

adv[0].val    = ADV_FLAGS;

adv[0].data[0] = LE_LIMITED_DISCOVERABLE | BR_EDR_NOT_SUPPORTED;

adv[1].len    = 16 + 1;

adv[1].val    = ADV_SERVICE_UUID128_COMP;

memcpy(adv[1].data, &test_uuid_main_vsc_service[0], 16);

// Tx power level

adv[2].len    = TX_POWER_LEN + 1;

adv[2].val    = ADV_TX_POWER_LEVEL;

adv[2].data[0] = bleprofile_p_cfg->tx_power_level;

// name

adv[3].len    = strlen(bleprofile_p_cfg->local_name) + 1;

adv[3].val    = ADV_LOCAL_NAME_COMP;

memcpy(adv[3].data, bleprofile_p_cfg->local_name, adv[3].len - 1);

bleprofile_GenerateADVData(adv, 4);

Scope

The scope is set to 100mV/div with 2.5ms/div.

DS0000.BMP  

Single ADV pulse, 2.5ms duration.  

DS0001.BMP

Multiple pulses, 2.5ms in duration at intervals of 100ms.

The smaller pulses located between the larger pulses are most likely due to other operations being run. The ramp up and ramp down shown just before and after a single pulse is most likely caused by the Bluetooth stack forcing the device to sleep when not advertising.

Excel

I've attached the Excel sheet for reference, here are the images of the graphs converted from voltage samples to actual current values. The scope's ADC measures 8 bit samples which are converted using the equation in the Excel document.

singlepulse.png

multipulse.png

0 Likes
15 Replies
MichaelF_56
Moderator
Moderator 250 sign-ins 25 comments on blog 10 comments on blog
Moderator

Appreciate the contribution whitephoenix92

Questions:

1. Was WICED Sense powered by battery or USB when you took the Tx current measurements?

2. Were any additional measures taken to isolate the Silicon Labs USB to Serial converter?

Note that we have also found ground plane issues on both TAG3 and WICED Sense that would cause irregular current measurements.

There is a new board coming out in Q3 that not only adds the ability to use an external DC-DC (i.e. 50% reduction), it also resolves some of the ground plane and component isolation issues found on the existing eval/dev boards.

The early measurements we have observed on this board are inline with the power numbers represented in the current BCM20737S Bluetooth Low Energy SiP Module Technical Reference

0 Likes
Anonymous
Not applicable

I think the original plan was to use a battery but instead we ended up using a 3.3V supply on the battery holder terminals.

No we didn't take extra measures to isolate the FTDI, I think since we powered it from the battery terminals we avoided the FTDI? I'd have to take a look at the schematic again.

Mostly I was just curious to know the duration of the adv tx event, peak current wasn't so much a concern but it will be nice having the ground plane issues worked out.

0 Likes
Anonymous
Not applicable

@mwf_mmfae

Hi, w.r.t. my response to whitephoenix92, is it the right way to achieve optimal efficiency for the on-chip 1.2V LDO with an external 1.8V DC-DC supply rather than 3V?  I am concerning majority of the time is just with light load.

Appreciated for any guidance on this subject.

0 Likes
Anonymous
Not applicable

Hi wong.jupiter,

Sorry for the late response, we would recommend the DC-DC, as mwf_mmfae said, our new TAG4 board, that is coming out soon, will have the ability to take more accurate power measurements with the external DC-DC.

Thanks,

Kevin

0 Likes
Anonymous
Not applicable

Hi Kevin,

thanks for the info.

0 Likes
Anonymous
Not applicable

This is a very good subject. With what you have in your excel sheet, majority of the time is at light load. So it is important to look at the efficiency at light load on the supply. However, most DC-DC efficiency is defined at its nominal loading. Another aspect is whether 3.3V supply is a good choice for the on-chip 1.2V LDO.  Should it be reduced to 1.8V?  I want to check with mwf_mmfae as well.

0 Likes
MichaelF_56
Moderator
Moderator 250 sign-ins 25 comments on blog 10 comments on blog
Moderator

I have asked j.t and kwang to respond as they are working more directly on the current measurements with the new eval board and will be able to provide more accurate technical guidance on tradeoffs associated with various voltage levels.

0 Likes
Anonymous
Not applicable

@mwf_mmfae

Thanks for your response. Could you also advise how the on-chip 1.2V LDO can be bypassed with an external 1.2V DC-DC?

0 Likes
MichaelF_56
Moderator
Moderator 250 sign-ins 25 comments on blog 10 comments on blog
Moderator
Bypassing the internal LDO is not possible using the SiP module in production today as VBAT is the only means to power the current SiP (recall we use SoCs on all of the dev boards and SoCs do not have this limitation). However, a new device will be released in Q3/Q4 which will allow the use of an external DC-DC (BCM20737L).


0 Likes
Anonymous
Not applicable

@mwf_mmfae

Do you mean I can use the BCM92073X_LE_KIT to by pass the on-chip 1.2LDO?  Greatly appreciated if you could provide some guidance on how to do so with the dev board.


So I can begin the works now while awaiting the BCM20737L.

0 Likes
MichaelF_56
Moderator
Moderator 250 sign-ins 25 comments on blog 10 comments on blog
Moderator

Unfortunately, you cannot use the TAG3/BCM92073X_LE_KIT to by pass the on-chip 1.2V LDO.

There will be another board released later this quarter (TAG4) that you can however use for this function.

0 Likes
JeCh_627636
Level 1
10 sign-ins 5 replies posted 5 sign-ins
Level 1

I checked the TAG3 board, and found it does keep the option to bypass the internal LDO and replace with the external one. Do we need BCM20737 firmware setting to disable the internal LDO for lower power comsumption when the external LDO is used ?

0 Likes
MichaelF_56
Moderator
Moderator 250 sign-ins 25 comments on blog 10 comments on blog
Moderator

We do not support an external LDO on the TAG3 board.

You will need to wait for the TAG4 to be relased later this quarter.

0 Likes
JeCh_627636
Level 1
10 sign-ins 5 replies posted 5 sign-ins
Level 1

Please confirm if it's needed with BCM20737 firmware setting to disable the internal LDO when the external LDO is used ?

0 Likes
Anonymous
Not applicable

Hello Jensen,

No firmware changes need to be made if an external LDO is used.

Thanks,

JT